How to erase EEPROM in an STM32L0-series part USING STM32CubeProgrammer?
The release notes for v2.2.0 say that feature is in there, but I can't seem to find it.I tried the "Full Chip Erase" feature & it cleared everything EXCEPT the EEPROM.
The release notes for v2.2.0 say that feature is in there, but I can't seem to find it.I tried the "Full Chip Erase" feature & it cleared everything EXCEPT the EEPROM.
Hi Everyone,I have a STM32L1 connected via USB in DFU-Mode.I'd like to write EEPROM, but trying to do so results in "Memory Limits Error".Using old DfuSe 3.0.6., this is possible... What am I missing? Is CubeProgrammer at all capable of writing EEPRO...
I have written a small driver code for the same to store different types of data types to a memory location.The link to my code is: Yadnik1/Eeprom-Emulation-driver-STM32 (github.com) and I have taken reference from here: STM32/FLASH_PROGRAM/F1 SERIES...
Good day. Faced such a problem. I wrote a loader for a non standard board, using stm32f476vgt MK, N25Q128A memory in extended SPI mode. All functions are tested in debugger mode. The data is written correctly, the memory is erased correctly, but veri...
Hallo,I am using STM32 CubeProgrammer and performed the "Full chip erase". after the Full chip erase some garbage value appears at EEPROM address (0x0808 0000 & 0x0808 0010) I have attached the image.Regards,Swapnil
Hi,I don't remember having this issue with v2.8 of STM32CubeProgrammer, but right now when I try to program a STM32L010 with an elf file that has the EEPROM part filed with values, both the GUI and the CLI fail to erase the EEPROM part of it, abortin...
When using the STM32CubeProgrammer 2.4.0 API to write the address 0x08080000 the API hangs (my program hangs). I tried the STM32CubeProgrammer software itself, if I choose the EEprom view (in the grid) and I modify any byte, when I validate modifica...
I want to know what is use of user data in option bytes programming?it helps to protect my firmware inside MCU like password or etc?
I tried to compile the example project STM32CubeProgrammer_2.2.0/api/project/Qt/STM32CubePrgAPI using mingw32, the project compiles perfectly but doesnt do anything at startup. When I compile it with mingw64 it works. STM32CubeProgrammer_2.4.0 does...