STM32CubeProgrammer (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Program for flashing over FD-CAN

Hi,I have ported the Open Bootloader to the STM32G431 and has flashed it and is able to communicate with it over FD-CAN. Is there any program out there that I can use to flash programs using the bootloader over FD-CAN? maybe the CLI version of the ST...

Unable to boot from BANK2

Hi, I am new to STM32G4 series. I am implementing dual bank firmware update on STM32G473 custom board. I've prepared two identical bin files(compiled to 0x08000000), and flashed them to 0x08000000 and 0x08040000.With options bytes:BFB2=0nBOOT0=1nBOOT...

THsu.1 by Associate II
  • 1399 Views
  • 8 replies
  • 0 kudos