STM32CubeProgrammer (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Program flashed in reverse (MSB LSB)

Hello, I am using an STM32F427ZIT6 on a custom board for my project and it was working perfectly until now. I was able to programming it with an ST-Link V2 + ST-Link Utility as expected.I was working on adding DMA to my code but one day my chip stopp...

0693W00000aJfkbQAC.png 0693W00000aJfl5QAC.png 0693W00000aJfljQAC.png
PSicl.2 by Associate
  • 761 Views
  • 3 replies
  • 0 kudos

Hello !!! Some strange error occured when I've tried to transfer a block data. First, Ithe processor received (by serial-DMA) 2006 bytes each time and this is repeated for 240 times resulting an array of 480,000 bytes

The processor is the STM32L4R5 and the SMT32CubeIDE versin 1.6. uint16_t US_Cksum,Trans_Pointer,USA_Data[2006],US_Trans[480000];uint32_t US_Pointer; US_Pointer is zeroed at the start of the program US_Cksum=0;// For Checksu...

INaka.1 by Associate III
  • 685 Views
  • 14 replies
  • 0 kudos