STM32CubeProgrammer (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! BOOT0/NRST control with DTR/RTS

Is it possible to use the DTR/RTS pins of a UART bridge (such as FT232RL) to automate entering the bootloader in system memory for flashing firmware using STM32CubeProgrammer? Has anybody achieved this?

jefflongo by Associate III
  • 2745 Views
  • 12 replies
  • 0 kudos

How to Enter boot loader in STM32H743BIT6 via USART1? pin BOOT0 is SET by SWITCH to "1" (VCC) (3.3V). the STM32H743BIT6 don't react to packets in USART1 from the STM32CubeProgrammer software.

How to Enter boot loader in STM32H743BIT6 via USART1?pin BOOT0 is SET by SWITCH to "1" (VCC) (3.3V).the STM32H743BIT6 don't react to packets in USART1 from the STM32CubeProgrammer software.

ZSade.1 by Associate II
  • 779 Views
  • 6 replies
  • 0 kudos

Resolved! How to enter ST USART Bootloader from Code?

Im trying to jump to bootloader section from my Code. I'm trying to update the firmware over USART with the intergrated bootloader. In my application I'm using USART2 (PA2/PA3) on a STM32L431CCU6 Microcontroller running native FreeRTOS. My Code to in...

_legacyfs_online_stmicro_images_0693W00000biZdlQAE.png

UART connection mode problems (2.13)

Platform: Windows 11 22H2 (x64)CubeProgrammer version: 2.13I've got 2 devices:HW Controller which uses dual FTDI drivers (2 COM ports; 1 port connected to ST microcontroller and 1 port connected to ESP32)HW Adapter which uses software virtual COM (ST...

Aelavin by Associate II
  • 362 Views
  • 0 replies
  • 0 kudos

Resolved! Program flashed in reverse (MSB LSB)

Hello, I am using an STM32F427ZIT6 on a custom board for my project and it was working perfectly until now. I was able to programming it with an ST-Link V2 + ST-Link Utility as expected.I was working on adding DMA to my code but one day my chip stopp...

0693W00000aJfkbQAC.png 0693W00000aJfl5QAC.png 0693W00000aJfljQAC.png
PSicl.2 by Associate
  • 758 Views
  • 3 replies
  • 0 kudos