STM32CubeProgrammer (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CubeProgrammer 2.12 - Operation exceeds memory limits

Hello Everyone,Here is my 512kB STM32L15xxE:     -------------------------------------------------------------------                      STM32CubeProgrammer v2.12.0     -------------------------------------------------------------------USB speed  : ...

0693W00000Y9FcEQAV.png
THein.3 by Associate II
  • 1701 Views
  • 3 replies
  • 0 kudos

STM32L152VD-X reserved memory space

Hello,I am using the STM32CubeProgrammer, version 2.10.0, and it does not detect the STM32L152VD-X reserved memory space, at address 0x0803000.The STM32CubeProgrammer detects the correct device ID which is 0x437 but does not detect the correct device...

VLock.2 by Associate
  • 435 Views
  • 4 replies
  • 0 kudos

Resolved! We have a problem downloading to the STM32L100 processor. It was programmed using STLink. Now we want to use STM32CubeProgrammer. Writing is not possible! It is not possible to change the RDP value either. If we use STLink, all is OK.

 10:55:25 : ST-LINK SN : 0034003E3137510339383538 10:55:25 : ST-LINK FW : V3J8M3B5S1 10:55:25 : Board    : STLINK-V3MODS 10:55:25 : Voltage   : 3.29V 10:55:25 : SWD freq  : 8000 KHz 10:55:25 : Connect mode: Under Reset 10:55:25 : Reset mode : Softwar...

Entony by Associate II
  • 343 Views
  • 2 replies
  • 0 kudos