STM32CubeProgrammer (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to boot from BANK2

Hi, I am new to STM32G4 series. I am implementing dual bank firmware update on STM32G473 custom board. I've prepared two identical bin files(compiled to 0x08000000), and flashed them to 0x08000000 and 0x08040000.With options bytes:BFB2=0nBOOT0=1nBOOT...

THsu.1 by Associate II
  • 944 Views
  • 8 replies
  • 0 kudos

Resolved! BOOT0/NRST control with DTR/RTS

Is it possible to use the DTR/RTS pins of a UART bridge (such as FT232RL) to automate entering the bootloader in system memory for flashing firmware using STM32CubeProgrammer? Has anybody achieved this?

jefflongo by Associate III
  • 2745 Views
  • 12 replies
  • 0 kudos

How to Enter boot loader in STM32H743BIT6 via USART1? pin BOOT0 is SET by SWITCH to "1" (VCC) (3.3V). the STM32H743BIT6 don't react to packets in USART1 from the STM32CubeProgrammer software.

How to Enter boot loader in STM32H743BIT6 via USART1?pin BOOT0 is SET by SWITCH to "1" (VCC) (3.3V).the STM32H743BIT6 don't react to packets in USART1 from the STM32CubeProgrammer software.

ZSade.1 by Associate II
  • 779 Views
  • 6 replies
  • 0 kudos

STM32CubeProgrammer page erase error

When using STM32CubeProgrammer to program STM32F103VET6, it is found that using the "page erase" function will erase the first page error by mistake (erase pages 1, 3, 5). Upon inspection, it is found that the page erase data sent by STM32CubeProgram...

_legacyfs_online_stmicro_images_0693W00000bjSPlQAM.png _legacyfs_online_stmicro_images_0693W00000bjSPWQA2.png
kaili.wu by Associate
  • 524 Views
  • 3 replies
  • 2 kudos

Easiest way to firmware update?

Hi all!So I'm looking for the easiest and fastest way to create a firmware update desktop app for an STM32 device (Arm Cortex M7). I would like to have something like CubeProgrammer, but way less functionalities (just programming/flashing). Being a c...

EAndr.2 by Associate II
  • 3319 Views
  • 5 replies
  • 0 kudos