Hello !I'm currently trying do make my own external loader for my board Mikromedia Capacitive 7.I have a STM32F746ZG MCU and the SST26VF064B 64Mbits Flash Memory.I want to make my external loader in order to store images in my external flash.I made d...
Heyin a project of us we are using the legacy STMFlashLoader to flash firmware on a STM32F103 via the system bootloader on UART1, but wanted to migrate to STM32CubeProgrammer now. In this application the PC (Win10) which runs STMFlashLoader/STM32Cube...
For everyday work I use ST-LINKs. Recently a customer gave me a JLINK for a board with a new QSPI flash chip, for this chip I could not find a ready external loader.Nevertheless the J-Flash software can program this chip, knowing only the the MCU and...
Hi. I'm developing with custom board which has a custom QSPI (EN25QX128A - 16Mbytes flash), so I need to make an external loader used by STM32CubeProgrammer.First I wrote a code that interacts with QSPI and it works fine.So I changed this code to ful...
I'm trying to create a loader for external flash. I cannot use IAR EWARM and the only examples I find use that. (e.g. https://github.com/STMicroelectronics/stm32-external-loader)I need this to work with GCC from a make file using LD linker scripts.An...
I downloaded latest STM32Flash loader for using the UART boot loaderbut it does not select and see the STM32H743Zi Nucleo boardi searched and found that version 2.8 which i am using does not have MAP file for the H7 Series The flash loader do support...
Hi everyone,I'm working on a custom external loader with an OSPI MX66LM1G45G memory and a STM32H7 A3.If I try to use my external loader in CubeProgrammer (in "Memory & file edition" tab) for reading OSPI at 0x90000000 for example, it works fine the f...