STM32CubeProgrammer (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

option byte of STM32H743VI was modified abnormal when debug by IAR, and if reset FZ_IWDG_STOP and FZ_IWDG_SDBY to default (1), the MCU can't run normally.

option byte of STM32H743VI was modified abnormal when I debug it by IAR, FZ_IWDG_STOP and FZ_IWDG_SDBY default value is 1, but after modified abnormal, I found the option bytes bits change to 0 except NRST_STOP_D1 bit, and then I try to reset all bit...

0693W00000WHRgfQAH.png 0693W00000WHRhEQAX.png
EXUE.2 by ST Employee
  • 220 Views
  • 0 replies
  • 0 kudos

SWV Hex Display

Is it possible to display the data from the ITM over the SWV viewer (NUCLEO-F401RE) in STM32CubeProgrammer in HEX? ITM_SendChar could be used to send just a 32-bit code, which takes far less CPU time than a printf-style debug output?

Amigo by Associate III
  • 169 Views
  • 0 replies
  • 0 kudos