How to erase EEPROM in an STM32L0-series part USING STM32CubeProgrammer?
The release notes for v2.2.0 say that feature is in there, but I can't seem to find it.I tried the "Full Chip Erase" feature & it cleared everything EXCEPT the EEPROM.
The release notes for v2.2.0 say that feature is in there, but I can't seem to find it.I tried the "Full Chip Erase" feature & it cleared everything EXCEPT the EEPROM.
Hello Everyone, II'm currently working with my Nucleo L073RZ board and so far my program built successfully but i cant upload it. Nonetheless, other programs are still able to run well on the board. I dont understand what i am doing wrong. I have rea...
Using ST-link V3.MCU: STM32L031First programming was ok. After disconnecting and reconnect with second device, nothing happen.Using same set of hardware, but changed software to ST-LINK Utility.Result: ok. Automatically programmed the second device.
Hi,I'm using latest STMCubeProgrammer/ST-Link-Utility releases. My goal is to provide the option bytes directly in the .elf/.hex file, so our manufacturing department only needs to download this file.I already managed to get the settings into the .el...
Hi,I am using STM32L071 micro controller for my product. We planned to flash the code using USART communication. The USART1 from MCU is connected to embedded system ( Nvidia Xavier NX ) using USB to UART converter. Then the MCU is put into boot mode ...
Hello everyone,I have made a custom board with STM32L072CBT6. All works fine when i use my board and program her with STLink.I would try to program my board through USB, to do that i have a uUSB connector on my board connected to my uC. To flash, i u...
HiI am struggling with the UART bootloader.My problem occurs when my firmware is greater than 128Kbyte. If it’s greater than 128Kbyte I get an error message with “operation exceeds memory limits.If I am doing the same with the ST-LINK interface there...
Hello,I cannot use the STM32CUBEprogrammer standalone program, however my programmer works just fine with stm32CUBEIDE V1.7. During programming in STM32cubeide the configuration is visible and it loads STM32cubeprogrammer V2.8 I copied the settings o...
Hi,I started developing a project for stm32l072cz. After seeing dfu mode working correctly I realized a problem. The objects that I program through the j-link Segger are serialized and when I go to upload the dfu file, the serialization is deleted. I...