Hi, i am looking for a small MCU with ARM trust zone, ROT, SFI and other security features similar to STM32L552.also fast SPI timing req similar to 401 family ( 401 reference only for timing)STM32F401CBU6, does not have the mentioned security feature...
On switching from secure to non-secure mode using a function pointer (with the cmse_nonsecure_call attribute) in STM32L562(ARM Cortex M33), general purpose registers R0-R4, R12 and floating point registers S0-S15 are not restored when back in secure ...
I use my own application to program different devices, arm in particular. Now, i'd like to support stm32L552. So, if TZEN = 0 it works fine. if TZEN = 1, DBANK = 1, SECWM1_PSTRT - set as secure, SECWM2_PSTRT - set as non-secure, RDP = 0xaa (level 0) ...
Hello,I want to use the security features included in the TFM in my application, I have followed UM2851, now,I have a better understanding for TFM and I succeed to implement it in STM32U585, to go further I want ot implement my own non-secure applica...
Hello,I want to use the security features included in the TFM in my application, I have followed UM2851, now,I have a better understanding for TFM and I succeed to implement it in STM32U585, to go further I want ot implement my own non-secure applica...
Hi,We are currently using an stm32l5 in our product and experimenting with a stm32L562E-dk and with the official TFM (https://git.trustedfirmware.org/TF-M/trusted-firmware-m.git master branch on the latest commit at this date.) The TFM is unmodified...
I'm attempting to use the serial bootloader to load a secure firmware image to an STM32L5 using STM32CubeProgrammer. I can successfully connect to the board in bootloader mode and perform a full-chip erase, but attempting to download the image (eithe...
I want to implement USART1 to the non-secure project of TFM_Appli in STM32L562 TF-M firmware package. I have add some code in secure project of TFM_Appli such as following:enum tfm_plat_err_t tfm_spm_hal_nvic_interrupt_target_state_cfg(void) { /* ...
I am using STM32L562-DK for my development, I am using SBSFU.In bootloader, I want to use timer 7 as an interrupt. I am configuring it as followingTIM_HandleTypeDef htim7;void TIM7_IRQHandler(void){ /* USER CODE BEGIN TIM6_IRQn 0 */ /* USER CODE E...