cancel
Showing results for 
Search instead for 
Did you mean: 

How to program stm32L552 using SWD interface

angry.sioux
Associate II

I use my own application to program different devices, arm in particular. Now, i'd like to support stm32L552. So, if TZEN = 0 it works fine.

if TZEN = 1, DBANK = 1, SECWM1_PSTRT - set as secure, SECWM2_PSTRT - set as non-secure, RDP = 0xaa (level 0) i cant read flash using SWD. STM32CubeProgrammer works perfectly in both cases.

I'd appreciate any help

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Imen.D
ST Employee

Hello @angry.sioux​ and welcome to the Community :)

Check if the SWD is mapped on the right pin.

I advise you to refer to this article: Security:How to disable TrustZone in STM32L5xx devices during development phase

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
angry.sioux
Associate II

Hi Imen,

>>Check if the SWD is mapped on the right pin.

I cannot read only the FLASH in case of TZEN = 1. But I read registers (CTRL_STAT, IDR...), can read OPTR, FLASHSIZE_BASE and so on. So, it;s not about a SWD pin.

>>I advise you to refer ....

I have read  Security:How to disable TrustZone in STM32L5xx devices during development phase and did not find an answer. Otherwise I would never reach out to for a favor.

Thank you

I found a way that made things a bit better.

There is WAIT response if i access to AP register. But.

If i read a register twice the error goes away.

f.e. schematically

//do not need to read, just write

write_register ( SELECT_REG, bank select for CSW_REG)

write_register ( SELECT_REG, bank select for TAR_REG) - error, WAIT

but

write_register ( SELECT_REG, bank select for CSW_REG)

read_reg(CSW_REG) - dummy read, enough for "no error", but returns trash.

read_reg(CSW_REG) - returns appropriate value

write_register ( SELECT_REG, bank select for TAR_REG) - no error, great

but

if i halt and reset core i got DHCSR_S_LOCKUP

Thanks for the quick reply and detailed answers to all inquiries. Thank you so much.

To simplify the process i'll split the problem into small pieces.

To write a some array i need to specify address (TAR) and tell CSW that i want to CSW_SIZE_32BITS, CSW_ADDRINC. After that i can write DRW in the loop as much as I need to. That is always how it has worked.

Now (in stm32L552 ) i see that i need to add dummy read after each iteration. Otherwise, i'm getting WAIT response.

The one question. Why?

You have been very helpful. Thank you. Thanks to your help i found out a workaround by adding idle request after writing. Though I still don't understand the difference with previous devices.

But now i faced with next problem. I halt the core and change PC (some code in this address). After start the core i get LOCKUP. (PC not 0xfffffffe) I do what used to do with numerous previous devices. I hope you'll help me in this case as you did it before. I have read you comments with great interest and pleasure. It's a pity that SWD pins on the right place.

Thank you so much.