STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

nDBOOT OB over UART broke after v2.14

Hello, This is a pretty straightforward bug report. For F767 Devices, when trying to configure dual boot mode over UART, the nDBOOT Option byte doesnt appear for Cubeprogrammer versions greater than v2.14 The typically workflow is1) uncheck nDBANK2) ...

dnugent by Associate II
  • 374 Views
  • 3 replies
  • 1 kudos

Resolved! STM32CubeProgrammer not working

I updated the STM3CubeProgrammer to version v2.22.0, and after restarting the app, it started showing a blank page. I was also not able to close the application directly. I had to end the task from the task manager. I uninstalled the latest version a...

image.png
abhi4 by Associate II
  • 625 Views
  • 4 replies
  • 2 kudos

USB DFU Firmware update while RDP1

Hello Team,Refering to this Thread : https://community.st.com/t5/stm32-mcus-products/updating-firmware-through-usb-dfu-with-readout-protection-level/m-p/838635We want to achieve same , Can I upgrade the firmware using USB DFU, with RDP set to level 1...

bsuthar by Senior
  • 759 Views
  • 7 replies
  • 1 kudos

Resolved! Error unable to read device id from rom table

Hello every people. I am new member. We have issue . We have one computer ( PC ) , it is working normaly, but when we setup for other devices , SMT32cube programmer not working.  Plz caution  , one PC working normaly, we received from custommer. New ...

DFU STM32H7S7L8 + External Loader

Hello,I'm working with the STM32H7S7L8 -DK and I need for final product to program the external OCTOSPI flash via usb DFU.So using V2.20.0 Cube programmer i'm able to use external memory loader to read and program the flash using SWDBut using the USB...

Hamady by Senior
  • 664 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.