2025-05-26 4:32 PM - edited 2025-05-29 1:49 PM
STM32CubeProg 2.19.0. STM32G041F8. MacOS 15.5. ST-Link.
I'm working on setting the brown-out rising, falling, and enable options on an STM32G041F8.
I started out by just using CubeProg to set the BOR_EN enable bit in the option bytes. Works correctly. It gives me the reaction I expected and I'm able to reconnect via CubeProg.
Next I wanted to set the BORF_LEV to something other than 3 so I can test my code. I set it to 1, hit Apply, Cube prog complains that the connection is lost and it has disconnected from the device, and now when I try and connect I just get:
17:13:46 : UR connection mode is defined with the HWrst reset mode
17:13:46 : ST-LINK SN : 31FF6A064D4E353828580643
17:13:46 : ST-LINK FW : V2J46S7
17:13:46 : Board : --
17:13:46 : Voltage : 3.31V
17:13:46 : Error: Unable to get core ID
17:13:46 : Error: No STM32 target found! If your product embeds Debug Authentication, please perform a discovery using Debug AuthenticationNo, I did not mess with the RDP values, just BORF_LEV.
CubeProg can't unbrick it. CubeIDE gets similar results. Unfortunately, for me, I duplicated the result in another processor so I thought I'd stop and reach out.
Any ideas as to how to unlock these things?
Thanks,
Andrei (your neighbour from The Great White North)
Solved! Go to Solution.
2025-07-07 4:24 PM
I figured that I should leave a message with the outcome of this posting.
The problem was real. I was able to brick a total of 5 processors. The problem was reasonably simple, the solution not.
The issue was that if you set the option bytes and don't do it correctly, the result is that the "Z" revision processors will erase the option bytes and lock the processor for read permanently. The later "Y" revision processors fixed this in that the option bytes are set to default and the processor is left in a recoverable condition. This is described in the errata.
Discussing this issue with ST, I was told a few times to be careful with the voltage applied to the processor during the option byte programming process. This wasn't a problem in my case as I was hooked to a power supply that was very stable. So watch that.
ST supplied some code for setting the brown-out and read-protect bytes that was not obvious, involved using the IWDT and lots of retry code, so I'll post it here for anybody else who wishes to set the option bytes on a G04 processor.
void MachineInit(void) {
/* OB Program structure */
FLASH_OBProgramInitTypeDef FLASH_OBInitStruct;
/*
* Arrange for the highest brown out detect possible.
*/
HAL_FLASHEx_OBGetConfig(&FLASH_OBInitStruct);
if (((FLASH_OBInitStruct.USERConfig & FLASH_OPTR_BOR_EN_Msk) != FLASH_OPTR_BOR_EN) || // BOR must be enabled
((FLASH_OBInitStruct.USERConfig & FLASH_OPTR_BORR_LEV_Msk) != BORR_LEVEL) || // Rising BOR must match needs
((FLASH_OBInitStruct.USERConfig & FLASH_OPTR_BORF_LEV_Msk) != BORF_LEVEL)) // Falling BOR must match needs
{
while (HAL_FLASH_Unlock() != HAL_OK) {}
while (HAL_FLASH_OB_Unlock() != HAL_OK) {}
FLASH_OBInitStruct.OptionType = OPTIONBYTE_USER;
FLASH_OBInitStruct.USERType = OB_USER_BOR_EN | OB_USER_BOR_LEV;
FLASH_OBInitStruct.USERConfig = OB_BOR_ENABLE | BORR_LEVEL | BORF_LEVEL;
while (HAL_FLASHEx_OBProgram(&FLASH_OBInitStruct) != HAL_OK) {}
SET_BIT(FLASH->CR, FLASH_CR_OPTSTRT);
while((FLASH->SR & FLASH_SR_BSY1) != 0) {}
MX_IWDG_Init();
while( HAL_FLASH_OB_Launch()!= HAL_OK)
{
HAL_PWR_EnterSTANDBYMode();
}
}
}There wasn't any explanation of why this code works, why they don't use the HAL or LL calls, and what the whole IWDG/Standby code is achieving, but it does work really really well.
Thanks to the FAE's at Arrow and ST for your help.
A
2025-05-27 1:38 PM
Okay, I officially hate this.
I figured that, since this topic got moved to the CubeProg list instead of the MCU products list, someone within ST had a thought that CubeProg is the problem. So I went ahead with my program. I wrote:
#define BORR_LEVEL OB_BOR_LEVEL_RISING_1
#define BORF_LEVEL OB_BOR_LEVEL_FALLING_1
void MachineInit(void) {
/* OB Program structure */
FLASH_OBProgramInitTypeDef FLASH_OBInitStruct;
bool needsLock = false;
/*
* Arrange for the highest brown out detect possible.
*/
HAL_FLASHEx_OBGetConfig(&FLASH_OBInitStruct);
if (((FLASH_OBInitStruct.USERConfig & FLASH_OPTR_BOR_EN_Msk) != FLASH_OPTR_BOR_EN) || // BOR must be enabled
((FLASH_OBInitStruct.USERConfig & FLASH_OPTR_BORR_LEV_Msk) != BORR_LEVEL) || // Rising BOR must match needs
((FLASH_OBInitStruct.USERConfig & FLASH_OPTR_BORF_LEV_Msk) != BORF_LEVEL)) // Falling BOR must match needs
{
(void) HAL_FLASH_Unlock();
(void) HAL_FLASH_OB_Unlock();
FLASH_OBInitStruct.OptionType = OPTIONBYTE_USER;
FLASH_OBInitStruct.USERType = OB_USER_BOR_LEV;
FLASH_OBInitStruct.USERConfig = BORR_LEVEL | BORF_LEVEL;
HAL_FLASHEx_OBProgram(&FLASH_OBInitStruct);
FLASH_OBInitStruct.OptionType = OPTIONBYTE_USER;
FLASH_OBInitStruct.USERType = OB_USER_BOR_EN;
FLASH_OBInitStruct.USERConfig = OB_BOR_ENABLE;
HAL_FLASHEx_OBProgram(&FLASH_OBInitStruct);
(void) HAL_FLASH_OB_Launch();
needsLock = true;
}
if (needsLock) {
/* Locks the option bytes block access */
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
}
}and it worked. CubeProg now shows that the enable bit is set and the BOR levels are set to 1.
So I change my code to the way that I need it:
#define BORR_LEVEL OB_BOR_LEVEL_RISING_3
#define BORF_LEVEL OB_BOR_LEVEL_FALLING_3no other changes. Run the program and the net result in CubeIDE is:
2025-06-03 9:01 AM
Hello @Andrei Chichak,
Apologies for the delayed response.
Could you please attempt to connect the target under reset using STM32CubeProgrammer?
Maryem.
2025-07-07 4:24 PM
I figured that I should leave a message with the outcome of this posting.
The problem was real. I was able to brick a total of 5 processors. The problem was reasonably simple, the solution not.
The issue was that if you set the option bytes and don't do it correctly, the result is that the "Z" revision processors will erase the option bytes and lock the processor for read permanently. The later "Y" revision processors fixed this in that the option bytes are set to default and the processor is left in a recoverable condition. This is described in the errata.
Discussing this issue with ST, I was told a few times to be careful with the voltage applied to the processor during the option byte programming process. This wasn't a problem in my case as I was hooked to a power supply that was very stable. So watch that.
ST supplied some code for setting the brown-out and read-protect bytes that was not obvious, involved using the IWDT and lots of retry code, so I'll post it here for anybody else who wishes to set the option bytes on a G04 processor.
void MachineInit(void) {
/* OB Program structure */
FLASH_OBProgramInitTypeDef FLASH_OBInitStruct;
/*
* Arrange for the highest brown out detect possible.
*/
HAL_FLASHEx_OBGetConfig(&FLASH_OBInitStruct);
if (((FLASH_OBInitStruct.USERConfig & FLASH_OPTR_BOR_EN_Msk) != FLASH_OPTR_BOR_EN) || // BOR must be enabled
((FLASH_OBInitStruct.USERConfig & FLASH_OPTR_BORR_LEV_Msk) != BORR_LEVEL) || // Rising BOR must match needs
((FLASH_OBInitStruct.USERConfig & FLASH_OPTR_BORF_LEV_Msk) != BORF_LEVEL)) // Falling BOR must match needs
{
while (HAL_FLASH_Unlock() != HAL_OK) {}
while (HAL_FLASH_OB_Unlock() != HAL_OK) {}
FLASH_OBInitStruct.OptionType = OPTIONBYTE_USER;
FLASH_OBInitStruct.USERType = OB_USER_BOR_EN | OB_USER_BOR_LEV;
FLASH_OBInitStruct.USERConfig = OB_BOR_ENABLE | BORR_LEVEL | BORF_LEVEL;
while (HAL_FLASHEx_OBProgram(&FLASH_OBInitStruct) != HAL_OK) {}
SET_BIT(FLASH->CR, FLASH_CR_OPTSTRT);
while((FLASH->SR & FLASH_SR_BSY1) != 0) {}
MX_IWDG_Init();
while( HAL_FLASH_OB_Launch()!= HAL_OK)
{
HAL_PWR_EnterSTANDBYMode();
}
}
}There wasn't any explanation of why this code works, why they don't use the HAL or LL calls, and what the whole IWDG/Standby code is achieving, but it does work really really well.
Thanks to the FAE's at Arrow and ST for your help.
A
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.