STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

qspi issue with MT25QL

tested an MT25QL NOR flash using STM32CubeProgrammer and an external loader.On the STM32 eval board (same MCU + same flash), read/write/erase works perfectly.On my custom board (same schematic and connections verified), I see an issue:Only alternate ...

QspiFlashMemoryDataWrite.png QspiFlashMemoryErase.png

Resolved! DFU mode read out protection

Hello, I am trying to connect to the STM32F072C8T6 microcontroller via USB in the STM32CubeProgrammer, however I am getting:"Device is under read out protection ! If you want to disable RDP please reconnect with Read Unprotect enabled"So, when I chec...

Draxter_0-1717577911683.png Draxter_1-1717578006569.png Draxter_1-1717580537175.png Draxter_0-1717580509580.png
Draxter by Associate II
  • 9116 Views
  • 18 replies
  • 12 kudos

STM32h743 external loader

I am using STM32h743XIH6 MCU with qspi flash MT25QL512ABB8ESF-0SIT same as STM32H743I-EVAL. when i try to load data to qspi flash using STM32CubeProgrammer and loader MT25TL01G_STM32H743I-EVAL.stldr provided by ST, data read/write working without any...

Resolved! Unable to flash with STM32CubeProgrammer

Hi,I just installed STM32CubeProgrammer v2.17.0 on Linux.When I connect to the board (tried with several different ones), I get the following error;flash loader cannot be loaded. FlashLoaderPath = /home/[yadayada]/bin/FlashLoader/0xI can read the fla...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.