Hello, Stm32cubeprogrammer installation does not proceed to the final stage, it remains at step 8 and is not completed. I tried the program on three different PCs with administrator rights, the result is the same, the installation does not complete.
Hello @Aziz BRIGUI Let me share an update on the issue.I tried to make a fresh installation with English (USA) Language Windows 11 and install the program, it was installed without any problems.My computer's language is Turkish, I added an English la...
Hello @Aziz BRIGUI This is the situation on the PC I use.I tried installing Windows 10 and Windows 11 on two different PCs without installing any programs, the result did not change, it remains at step 8. I think it might be regional or Windows langu...