STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! DEV_USB_COMM_ERR for REAL St-link V2

I bought an ST-link V2 from amazon, this error occured, fearing it may be counterfeit, I then bought another St-link v2 from STM website itself so there is no way it is fake, but the same error still occured. I am on Mac M3 using Cubeprogrammer. Ther...

OWENL by Associate II
  • 1416 Views
  • 8 replies
  • 2 kudos

STM32N6 .tsv file with application

Hello,What is the correct layout for the .tsv file for the STM32N6 with application?In this tutorial the FlashLayout.tsv is shown, however it only has the FSBL program in it. I cannot figure out what Id to use for the Appli (also Appli non secure), i...

Tuomas95 by Associate III
  • 363 Views
  • 3 replies
  • 0 kudos

Resolved! Cannot connect to STM32H747BIT6 anymore

I have been running into an issue with the cubeprogrammer very recently where I am unable to connect to my MCU anymore. I get the following log: using v2.2212:41:28 : STM32CubeProgrammer API v2.22.0 | Windows-64Bits12:43:17 : UR connection mode is de...

peter627 by Associate II
  • 743 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.