STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32CubeProgrammer J-Link issue

I'm trying to use the STM32CubeProgrammer with the newly supported J-Link settings, but can't seem to get it to work.I'm using:STM32CubeProgrammer: v2.17.0STM32H573I-DKSEGGER J-Link PLUS: SEGGER J-Link Commander V8.10c (Compiled Oct 16 2024 16:20:30)...

Resolved! Unable to connect to STM32H523

Hi,I am trying to connect to a STM32H523RET MCU via SWD using a J-link Debugger (CubeProgrammer v2.17.0).Reading the Product ID fails, so I get asked to select the MCU manually.Unfortunately the list does not contain any STM32H52x MCU But when I am t...

WhoIsJohnGalt_2-1727295663441.png WhoIsJohnGalt_3-1727295706101.png WhoIsJohnGalt_0-1727295541006.png WhoIsJohnGalt_1-1727295559401.png

Resolved! Cube programmer halts CPU

Hi, I hope someone can help me with this.I am using STM32CubeProgrammer 2.16.0 with an NUCLEO-H563ZI and Ubuntu 23.10. Programming, reading Registers seems to work. STM32CubeProg halts or runs my running or halted MCU approx every second depending on...

STM32CubeProgrammer 2.18.0 released

STM32CubeProgrammer v2.18.0 release information New features:  Added the support for the STM32N6 series– OTP programming– External memory programming– Serial boot via USB/UART– FSBL signature with stm32header V2.3 through the signing tool• Added the ...

Resolved! STM32F746G Discovery: Failed to erase memory

Originally a reply here: https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/stm32f746g-discovery-what-is-the-difference-between-cu2-and-cu4/m-p/746537/highlight/true#M40704  - moved to a new Thread for the new question. Thank you so much for you...

BA2 by Associate II
  • 1851 Views
  • 2 replies
  • 1 kudos

STM32CubeProgrammer 2.17.0 released

STM32CubeProgrammer v2.17.0 release information New features:• Added the support for the STM32MP25xx microprocessors in the STM32MP2 series – Flash memory and OTP programming, SSP support Added the support for devices in the STM32WB0 series: STM32WB0...

Resolved! STM32G071CBU6 DFU and UART Bricking issue

Just startet my small modbus therrmocouple project and im facing the issue with STM32G071CBU6.       First of all im not abble to connect via DFU usb, device isnt recognize i try reinstal stmCubeProgrammer, didnt change anything. Then try install dri...

stm32 dfu issue.png