cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer 2.16 - cannot program MCU by USB

STeve-o
Associate

Hello,

After installing STM32CubeProgrammer v2.16, I was unable to program a STM32F412 by USB (in DFU mode).

I've never had a problem doing this and after uninstalling v2.16 and installing v2.15, everything worked fine.

This problem was also confirmed by my colleague who is in a different location.

 

Here is the log for v2.15:

12:22:33 : STM32CubeProgrammer API v2.15.0 | Windows-64Bits
12:22:48 : UR connection mode is defined with the HWrst reset mode
12:22:48 : USB speed : Full Speed (12MBit/s)
12:22:48 : Manuf. ID : STMicroelectronics
12:22:48 : Product ID : STM32 BOOTLOADER
12:22:48 : SN : 3141B9563238
12:22:48 : DFU protocol: 1.1
12:22:48 : Board : --
12:22:48 : Device ID : 0x0441
12:22:48 : UPLOADING OPTION BYTES DATA ...
12:22:48 : Bank : 0x00
12:22:48 : Address : 0x1fffc000
12:22:48 : Size : 16 Bytes
12:22:48 : UPLOADING ...
12:22:48 : Size : 1024 Bytes
12:22:48 : Address : 0x8000000
12:22:48 : Read progress:
12:22:48 : Data read successfully
12:22:48 : Time elapsed during the read operation is: 00:00:00.005
12:22:56 : Memory Programming ...
12:22:56 : Opening and parsing file: V125_20230420.hex
12:22:56 : File : V125_20230420.hex
12:22:56 : Size : 254.96 KB
12:22:56 : Address : 0x08000000
12:22:56 : Erasing memory corresponding to segment 0:
12:22:56 : Erasing internal memory sectors [0 4]
12:22:57 : erasing sector 0000 @: 0x08000000 done
12:22:57 : erasing sector 0001 @: 0x08004000 done
12:22:57 : erasing sector 0002 @: 0x08008000 done
12:22:58 : erasing sector 0003 @: 0x0800c000 done
12:22:59 : erasing sector 0004 @: 0x08010000 done
12:22:59 : Erasing memory corresponding to segment 1:
12:22:59 : Erasing internal memory sector 6
12:23:01 : erasing sector 0006 @: 0x08040000 done
12:23:01 : Erasing memory corresponding to segment 2:
12:23:01 : Erasing internal memory sector 7
12:23:02 : erasing sector 0007 @: 0x08060000 done
12:23:02 : Erasing memory corresponding to segment 3:
12:23:02 : Not flash Memory : No erase done
12:23:02 : Download in Progress:
12:23:07 : File download complete
12:23:07 : Time elapsed during download operation: 00:00:11.188
12:23:07 : Verifying ...
12:23:07 : Read progress:
12:23:08 : Download verified successfully

 

Here is the log for v2.16:

12:18:04 : STM32CubeProgrammer API v2.16.0 | Windows-64Bits
12:18:10 : UR connection mode is defined with the HWrst reset mode
12:18:10 : USB speed : Full Speed (12MBit/s)
12:18:10 : Manuf. ID : STMicroelectronics
12:18:10 : Product ID : STM32 BOOTLOADER
12:18:10 : SN : 3141B9563238
12:18:10 : DFU protocol: 1.1
12:18:10 : Board : --
12:18:10 : Device ID : 0x0441
12:18:10 : UPLOADING OPTION BYTES DATA ...
12:18:10 : Bank : 0x00
12:18:10 : Address : 0x1fffc000
12:18:10 : Size : 16 Bytes
12:18:10 : UPLOADING ...
12:18:10 : Size : 1024 Bytes
12:18:10 : Address : 0x8000000
12:18:10 : Read progress:
12:18:10 : Data read successfully
12:18:10 : Time elapsed during the read operation is: 00:00:00.004
12:18:40 : Memory Programming ...
12:18:40 : Opening and parsing file: V125_20230420.hex
12:18:40 : File : V125_20230420.hex
12:18:40 : Size : 254.96 KB
12:18:40 : Address : 0x08000000
12:18:40 : Erasing memory corresponding to segment 0:
12:18:40 : Erasing internal memory sectors [0 4]
12:18:40 : sector 0000 does not exist
12:18:40 : sector 0001 does not exist
12:18:40 : sector 0002 does not exist
12:18:40 : sector 0003 does not exist
12:18:40 : sector 0004 does not exist
12:18:40 : Erasing memory corresponding to segment 1:
12:18:40 : Erasing internal memory sector 6
12:18:40 : sector 0006 does not exist
12:18:40 : Erasing memory corresponding to segment 2:
12:18:40 : Erasing internal memory sector 7
12:18:40 : sector 0007 does not exist
12:18:40 : Erasing memory corresponding to segment 3:
12:18:40 : Not flash Memory : No erase done
12:18:40 : Download in Progress:
12:18:43 : File download complete
12:18:43 : Time elapsed during download operation: 00:00:02.584
12:18:43 : Verifying ...
12:18:43 : Read progress:
12:18:43 : Error: Data mismatch found at address 0x080045BC (byte = 0x30 instead of 0x70)
12:18:43 : Error: Download verification failed

 

You can see many problems with the v2.16 log.

Thank you in advance for your help.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
STTwo-32
ST Employee

Hello @STeve-o 

A simular problem was reported on an STM32L4. I will add your case to the internal escalation ticket for correction. Thank you so much for reporting.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

This issue is confirmed and reported on the 178135 and it will be solved on the next Releases.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Is there an ETA for the next release?  I can't download an earlier version of this program on your website.