Skip to main content
JU_it
Senior
April 8, 2024
Question

Can't install V2.16.0 in Debian/Raspbian Linux - installer insta-quits

  • April 8, 2024
  • 2 replies
  • 1508 views

Per the title really - I've just tried to install the Linux version on a raspberry pi running Raspbian / Debian 11.7 'Bullseye' and, well, NOTHING happens.

If I click 'SetupSTM32CubeProgrammer-2.16.0.linux' nothing happens at all, if I select "execute in terminal" I get a brief flash of a terminal window, a mystery file of 0 bytes is created (named with a single unicode character and 'P').

If I run it from the terminal I get:

$ ./SetupSTM32CubeProgrammer-2.16.0.linux
-bash: ./SetupSTM32CubeProgrammer-2.16.0.linux: cannot execute binary file: Exec format error

 

 

Also why is a tool for programming microcontrollers a 286Mb download for which we must give ST our blood type and inside leg measurement just to be allowed to download it? :flushed_face:

2 replies

Maryem
ST Employee
April 9, 2024

Hello @JU_it ,

 

Currently STM32CubeProgrammer does not support ARM platforms. This request has already been raised to the development team. I will make sure to keep you informed of any advancements regarding this issue.

Internal ticket number: 162152 (This is an internal tracking number and is not accessible or usable by customers).

 

Maryem.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Maxime_BELAVAL
ST Employee
April 16, 2026

Hello,
Thank you for your patience, we know this has been a long-awaited request!

We're happy to share that Raspberry Pi support for STM32CubeProgrammer will be available in June 2026 with version 2.23.

Please refer to this Developer News for more information: [Coming June 2026] Raspberry Pi support for STM32CubeProgrammer

We also encourage you to share your feedback with us by commenting on the Dev News, as it helps us prioritize future improvements and developments.

Thank you all,
Max