cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer 2.16.0 crashing in SWV

krasl
Associate

Hello,

I'm using STM32CubeProgrammer version 2.16.0. The debugging works fine, but if the connection with the target is lost or probably some bad message is received on the client side, the application crashes. So in the first place I can't even see the last SWO messages that were received from the target.

Hardware: STM32U585 - SWD - HW Reset - ST-Link V2.0 ISOL @ V2J43S7

System log attached.

 

thx,

- Martin

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0