STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32G0 unable to connect via SWD

I tried to connect the STLink to the STM32G030K6T6 by connecting SWCLK SWDIO VDD and GND pins, but the STM32CubeProgrammer can't detect the MCU.I also tried to check with the logic analizer the pins and there is only a little signal from the stlink b...

FMill.2 by Associate
  • 2749 Views
  • 3 replies
  • 0 kudos

STM32CubeProgrammer won't erase target device flash.

Hi all. I am using STM32CubeProgrammer with an STM32G474VET6 target system on a Windows 10 box with a USB-connected STLink module. The programmer is v2.10.0, and the STL firmware is v2J3757.My problem is that the Cube programmer doesn't seem to be ab...

SDiMo.1 by Associate
  • 3840 Views
  • 2 replies
  • 0 kudos