STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

What do "Download" and "Upload" mean?

In the Good Old Days, "Download" always meant sending stuff to the Target (ie, programming), and "Upload" meant getting stuff from the Target (reading).But the ones at Arduino have messed that up, saying "Upload" for programming the Target.eg, https:...

External Flash loader not working with Cube Programmer

Followed STM tutorial on the subject. This is custom board STM32G484 with Winbond 25q128jvsq. Memory can read, erased and written to. It passes all the tests in quad mode (4 IO lines). However Programmer reads only single line, hence rather all FF's ...

ASmer.1 by Associate II
  • 1712 Views
  • 2 replies
  • 0 kudos

I have created an External Loader for my custom board with IS25LP064D connected to an STM32H730IB via OCTOSPI 1. I am able to successfully Read, Sector Erase and Mass Erase via Cube Programmer BUT Programming a Binary File into the Flash returns ERROR.

Dear ST Community,Thank you for taking the time to go through this :)I had created the External Loader by following the Tutorial uploaded by STM on Youtube.Link to the Tutorial: https://youtu.be/XqCq0xtQmbII created the External Loader after seeing s...

0693W00000Kd6fIQAR.png 0693W00000Kd6fXQAR.png

Resolved! STM32CubeProgrammer connection over UART error

Hi, I've some problem using SMT32CubeProgrammer. i am trying to connect via uart to micro stm32g491 but i receive some error messages. 15:21:34:034 : RTS low 15:21:34:034 : DTR low 15:21:34:171 : Serial Port COM15 is successfully opened. 15:21:34:172...

ERazz.3 by Associate II
  • 8428 Views
  • 12 replies
  • 0 kudos