STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32H747I-DISCO and STM32CubeProgrammer 2.5.0

Hi All,I have STM32H747I-DISCO board with a built-in STLink-V3E. I am trying to falsh the MCU, but no matter what I do, I cannot get STM32CubeProgrammer 2.5.0 to recognise the board.I plug the board into Win10 PC via a micro-USB cable in the ST-Link-...

YMill.1 by Associate II
  • 1926 Views
  • 4 replies
  • 0 kudos

STM32CubeProgrammer not clearing the Option Bytes on STM32H7B3i-DK. I can not load any code and stuck. Is it possible to clear these bytes with STM32CubeProgrammer and if so how?

STM32CubeProgrammer not clearing the Option Bytes on STM32H7B3i-DK. I can not load any code.Is it possible to clear these bytes with STM32CubeProgrammer and if so how? Below is the error that I am getting.13:58:53 : Time elapsed during the read opera...

onio by Senior
  • 1539 Views
  • 2 replies
  • 0 kudos

Resolved! NEWBIE Unable To Debug Or Run Simple Blinky Project

Hi everyone, I recently got a Nucleo board (STM32L476RG) to introduce myself to the stm32 mcu and I've installed the stm32cubeide alongside it. I've been trying to run a simple blinky project for the past hour but I keep getting this message, "Waitin...

0693W000003Q2BPQA0.jpg
TNguy.18 by Associate II
  • 2543 Views
  • 4 replies
  • 0 kudos