STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

How to disable Core M4 Boot? Is it possible to work on debug mode with one core without disable one of them ?

I cannot install properly stm32cubeprogrammer after installation step 6 it is not installing even if I use an individual laptop. So I could not be able to over the stm32cubeprogrammer. I didn't find a topic about installation problems for stm32cubepr...

AI1 by Associate II
  • 2088 Views
  • 2 replies
  • 0 kudos

Resolved! [SOLVED] Problem running STM32CubeProgrammer

When running the program STM32CubeProgrammer, an error message appears, saying:"CubeProgrammer_API or one of its dependencies is missing. Please try reinstalling the program of check your java architecture". However I have the lastest JAVA SE Run Tim...

protect sector when upload in dfu

Hi,I started developing a project for stm32l072cz. After seeing dfu mode working correctly I realized a problem. The objects that I program through the j-link Segger are serialized and when I go to upload the dfu file, the serialization is deleted. I...

Error: Data mismatch found at address 0x08001504 (byte = 0xF7 instead of 0x7B) Error: Download verification failed

I've connected an STM32F407-G-DISC1 board to debug a DIY-MORE breakout board. The debuggee is connected via SWDCLK,SWDIO, NRST to the STLINK-SWD interface of the DISC1 board. Discovery jumpers are off, ST-LINK enabled.I'm loading a blinky app but whe...

STM32CubeProgrammer graphical Windows working, same hardware STM32CubeProgrammer Cmd Line is not working,

CubeProgrammer under Windows (graphical Version) is working fine. CubeProgrammer with Cmd Line brings error:Output     -------------------------------------------------------------------                     STM32CubeProgrammer v2.10.0    ------------...

0693W00000KdYTeQAN.jpg 0693W00000KdYUDQA3.jpg
franz2 by Associate III
  • 1890 Views
  • 1 replies
  • 0 kudos

ST32F413 Won't Program in Cube Programmer?

I have two identical pre-production PCBs containing fresh, unprogrammed 32F413VGT micros from our distributor. One board will program just fine but CubeProgrammer says "can't erase device!" when I try to program the other board.After first scanning ...

JOlso.12 by Associate III
  • 1353 Views
  • 2 replies
  • 0 kudos