STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! Does Registers work in STM32Cube Programmer?

I am trying to use Registers in STM32CubeProgrammer to change the setting of GPIOB, but whenever I change a value. it just gets changes back to the value it had before! Is this because Registers is still in BETA or am I doing something wrong?

KMoel.1 by Associate II
  • 2294 Views
  • 7 replies
  • 0 kudos

Resolved! Did ST break SysTick in the last update? It used to work. Now it crashes because I think the interrupt vector is not set. Is this one of those known errors? How do I fix it?

When the SysTick interrupt fires the debugger quits. I cannot figure out where the NVIC_SetVector statement is for the SysTick. I think it is not set. But I can not find the vector table in the debugger to know for sure. This used to work, But when I...

KiptonM by Lead
  • 11683 Views
  • 30 replies
  • 0 kudos

STM32CubeProgrammer STM32G474 option bytes

Dear allI think the description is wrong or BOOT0/BOOT1 is swapped - see attachments.If the option bytes are programmed as shown under STM32CubeProgrammer.png, the controller boots from flash.Thanks in advance,Franz

FWege.1 by Associate III
  • 2200 Views
  • 1 replies
  • 1 kudos

Resolved! Write OTP lock bytes using ST-LINK/V2

Hi,i try to write the OTP area lock bytes using the ST-LINK/V2 programmer with the ST STM_Programmer_CLI tool included in the STM32CubeProgrammer software package.I can successfully write to the OTP area blocks using the -w32 command but if i try to ...

YWilk.1 by Associate II
  • 8278 Views
  • 17 replies
  • 0 kudos