STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! How do i need to create .bin file for an QSPI memory?

I am a beginner and I do according to this video "External Qaspi Loader How to - 05 - Qspi Driver Coding" https://youtu.be/XqCq0xtQmbI I uploaded the project "EXTERNAL QSPI Loader" to stm and now question about .bin fileHow to create a data file to b...

DK.7 by Senior
  • 3601 Views
  • 7 replies
  • 0 kudos

Resolved! STM32CubeProgrammer 2.10.0 and 2.11.0 External loader bug: if the EL's filename has more tha one dot (one dot only for its extension name) STM32CubeProgrammer goes in error.

If the name (filename) of module has more than one dot ( "." ) the STM32CubeProgrammer can list it in the external loder (EL) selection, but when STM32CubeProgrammer tries to use the module it fails (it generates an error).For example this EL name ge...

Resolved! Extraction of bin file from microcontroller

Hey, sorry, I am pretty new to this. I have a rather basic question. I took apart a module that I have, within which there is STM32 microcontroller (part marking: STM32F103T8U77BA7E93PHL739). I want to know if it's possible to use the IDE to extract ...

BTay.1 by Associate II
  • 24265 Views
  • 30 replies
  • 1 kudos

Resolved! Issues with GDB Server...Need help!!

I have an STLINK-V3SET connected to a Seeed Lora-E5. I also have a Nucleo L476 developement board with on-board STLINK. On the Seeed board I am able to connect STM32CubeProgrammer and have loaded a file. I cannot connect however STM32CubeIDE as I get...

0693W00000QKIxAQAX.png 0693W00000QKIy3QAH.png
SWenn.1 by Senior III
  • 1398 Views
  • 2 replies
  • 0 kudos

Resolved! auto start SWV

Hi,the Serial wire viewer (SWV) has a command-line option. This only launch the viewer and the user has to press R to start.Is it possible to directly start the SWV?Or is there a shell trick for this? - Thomas*****************************************...

T B by Associate II
  • 1963 Views
  • 1 replies
  • 0 kudos