STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32H750 externalloader fails on SystemClock_Config.

Hi. I'm developing with custom board which has a custom QSPI (EN25QX128A - 16Mbytes flash), so I need to make an external loader used by STM32CubeProgrammer.First I wrote a code that interacts with QSPI and it works fine.So I changed this code to ful...

YNam.1 by Associate
  • 1350 Views
  • 1 replies
  • 0 kudos

Resolved! CubeProgrammer 2.11.0 Bootloader revision reading bug

Hello,I have updated CubeProgrammer to its latest revision (2.11.0) and it finally displays the bootloader version in the target information box (with a Nucleo-G070RB).However it keeps reading the bootloader revision every 1 second, as shown by the l...

Kraal by Lead
  • 2481 Views
  • 5 replies
  • 1 kudos

In cubeprogrammer unbale to add start address

Hello,I am working on NUCLEO-H7 board . Its dual core CM7 and CM4. When I Erase the full flash then I click into erase and programming option but I unable to add start address . The core M7 is get programming , but in Core M4 i unable to do programmi...

0693W00000QMvVYQA1.png
MDeva.1 by Associate II
  • 4136 Views
  • 8 replies
  • 1 kudos

Not able to connect with stm32 cube programmer

Dear sir, I want to connect my stm32 board with stm32 cube programmer. ​but there is some issue, 1.i am able to read the device number , but the connect led does not turn green 2. Then I get messages of check boot configuration and serial port.3. I...

NSane.1 by Associate II
  • 3488 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.