STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32U575/STM32U585 Programming time different

Hi Everybody,     Now i met an issue for STM32U575/STM32U585 Programming time different, below is my test log, i don't why get the different time, since i do the erase in any time. The blank chip programming time is 34s, and NOT BLANK chip programmin...

Yongquan by Associate II
  • 287 Views
  • 6 replies
  • 0 kudos

Resolved! STM32CubeProgrammer crash on files selection

Hi everyone,I’m experiencing a new issue with STM32CubeProgrammer and I’m wondering if anyone else has run into the same problem.Starting today, every time I try to select a file (for example, when choosing a .bin or .hex to flash), the program freez...

LMenc.1 by Associate II
  • 705 Views
  • 7 replies
  • 2 kudos

stlink-gdb-server connection mode

When we want to debug only the M7 core, we use the following line and connect from VsCode:/c/ST/STM32CubeIDE_1.14.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_2.2.200.202505060755/tools/bin/ST-LINK_gdbserver.e...

CNien by Associate II
  • 695 Views
  • 2 replies
  • 1 kudos

STM32N657X0-Q ST-Link error (DEV_CONNECT_ERR)

Hey ho everyone I'm a Noob with all this, just surface level knowledge.I'm on Linux ((Ny)arch btw.) newest version. First everything worked switched boot mode (cant remember if boot 1 or 0 as no combination works now) and i could connect. Then i want...

Hitori by Associate
  • 502 Views
  • 1 replies
  • 0 kudos

Need help with CubeProgrammer CLI syntax

Hello,STM32L4+, CubeProgrammer 2.21, ST-Link V2, Windows 10I need to do:* Full flash erase* Write Application image (.hex or .bin)* Write Bootloader image (.hex or .bin)* Set RDP level 1* Start the application at the Bootloader start address.-I am su...

NArnd by Associate III
  • 1354 Views
  • 20 replies
  • 5 kudos

Resolved! CubeProgrammer won't work properly

After updating and restarting my PC with Windows 10, my old version of CubeProgrammer would not open at all. The version number is unknown. Other STM32 software works without any issue such as CubeMX and CubeIDE.I then tried installing the latest ver...

AL_0-1769186665936.png
AL by Associate III
  • 446 Views
  • 6 replies
  • 4 kudos