STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32U575/STM32U585 Programming time different

Hi Everybody,     Now i met an issue for STM32U575/STM32U585 Programming time different, below is my test log, i don't why get the different time, since i do the erase in any time. The blank chip programming time is 34s, and NOT BLANK chip programmin...

Yongquan by Associate II
  • 348 Views
  • 6 replies
  • 0 kudos

Resolved! STM32CubeProgrammer crash on files selection

Hi everyone,I’m experiencing a new issue with STM32CubeProgrammer and I’m wondering if anyone else has run into the same problem.Starting today, every time I try to select a file (for example, when choosing a .bin or .hex to flash), the program freez...

LMenc.1 by Associate II
  • 760 Views
  • 7 replies
  • 2 kudos

stlink-gdb-server connection mode

When we want to debug only the M7 core, we use the following line and connect from VsCode:/c/ST/STM32CubeIDE_1.14.1/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_2.2.200.202505060755/tools/bin/ST-LINK_gdbserver.e...

CNien by Associate II
  • 746 Views
  • 2 replies
  • 1 kudos

STM32N657X0-Q ST-Link error (DEV_CONNECT_ERR)

Hey ho everyone I'm a Noob with all this, just surface level knowledge.I'm on Linux ((Ny)arch btw.) newest version. First everything worked switched boot mode (cant remember if boot 1 or 0 as no combination works now) and i could connect. Then i want...

Hitori by Associate
  • 533 Views
  • 1 replies
  • 0 kudos

Need help with CubeProgrammer CLI syntax

Hello,STM32L4+, CubeProgrammer 2.21, ST-Link V2, Windows 10I need to do:* Full flash erase* Write Application image (.hex or .bin)* Write Bootloader image (.hex or .bin)* Set RDP level 1* Start the application at the Bootloader start address.-I am su...

NArnd by Associate III
  • 1516 Views
  • 20 replies
  • 5 kudos