User Activity

Hello everyone,I'm currently working on a USB Type‑C Power Delivery design using the STM32U575VGT6Q and the TCPP01‑M12. According to the TCPP01‑M12 datasheet and the example from the UM2581 STM32L5 Nucleo Board, the DB pin should be connected to a GP...
I am trying to use CLion to program STM32 MCUs as an alternative to other IDEs. For flashing and debugging, I want to use the Embedded GDB Server provided by ST, specifically ST-LINK_gdbserver.exe.I prefer not to use OpenOCD because I have found it t...
Hello everyone,I am working with the STM32G0B1KEU6 microcontroller, which comes in a 32-pin package featuring only ports A, B, and C. According to AN2606, the internal bootloader uses the following pins:FDCAN1_Rx pin: Input PD0, used in alternate pus...
Is there a way to Upgrade STM32CubeIDE or Pro License for this Software?  It's very anoying e.x. when I try to debug something and the max possible breake point number is 8 or something. Is there is option to avoid this limitations or do you use anot...
Hello together,does anyone know how I can implement multiple USB device classes on a STM32?I want to use the CDC so a VCP and the DFU class so I can communicate with my chip and drive an update if needed. I am working with a STM32L452RE.It must be po...
Kudos from
Kudos given to