STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RSA Pair Key generation on STM32L496

Hello,I am working on STM32L496, that does not have an AES hardware encryption, and i wanted to generate a pair of RSA Keys, public and private keys.I wonder if i can use mbedTLS or any library to do so or not?If i can do it, is there any example or ...

aybood by Associate
  • 1538 Views
  • 1 replies
  • 0 kudos

STM32H743 RDP Level 1

Hii dont fully get what is possible under RDP Level1 on STM32H743. I have a application which loads credentials into SRAM2. AN5156 writes that debug accesses to SRAM2 are forbidden. As it seems i can still read SRAM2 via STM32CubeProgrammer but the d...

bgi95 by Associate
  • 3276 Views
  • 1 replies
  • 0 kudos

Erase non secure page from secure domain

Hi,we are developing a firmware on the STM32U575QG MCU. Trustzone is enabled and configured as follows (DBANK active).Flash memory size is 1MB, with DBANK active. So, from my understanding, it should be two different bank, each one composed by 64 pag...

alessandromorniroli_0-1687169218695.png alessandromorniroli_1-1687170571072.png

Resolved! STM32 CRYPTOGRAPHIC FIRMWARE LIBRARY

Hello, I would like to install the stm32 cryptographic firmware library to use with the STM32F030K6Tx.I download the latest version of the library the 4.1.0 from https://www.st.com/en/embedded-software/x-cube-cryptolib.html.I followed the guide https...

LMalv.1 by Associate II
  • 4191 Views
  • 4 replies
  • 1 kudos

Resolved! Can't activate readout protection using option bytes

HiI try to activate readout protection using jlink/jflash.The read out protection is level 0 (0xaa on last bytes of option byte currently 0xDFFFE1AA), I want to set level 1, using 0x00 value instead of AA.After flashing my binary, lock and optlock pr...

GBout1 by Associate
  • 4094 Views
  • 3 replies
  • 0 kudos

Resolved! DIfference in results based on different AES mode

If I use AES mode CRYP_CR_ALGOMODE_AES_CBC, the decryptedText array does not match with the last 3 uint32_t values in the array. Same goes with ECB mode. However, when GCM or CCM modes are used, the decrypted data is same as the plain text. I could n...

abtom87 by Associate II
  • 4981 Views
  • 9 replies
  • 3 kudos