2022-09-28 12:13 PM
I shall just write a function in software but I would be interested to know if it is supported or not by the CRC peripheral hardware.
STM32 cube MX configurator does not allow you to choose X7 for the 7bit (8 term) polynomial described on page 21 of this datasheet?
It is also prevented by a length check on line 111 of stm32l4xx_hal_crc_ex.c
(case CRC_POLYLENGTH_7B)
"https://www.sciosense.com/wp-content/uploads/documents/SC-000897-DS-7-ENS210-Datasheet.pdf"
Thank You
2022-09-28 12:39 PM
Should support 7, 8, 16, 32-bits with proper incantations.
Demonstrably capable of 5 and 24-bit CRC with ingenuity. Depends a lot on how the data presents, and methods likely applicable for 3 thru 31-bit.
2022-09-28 1:13 PM
The 17-bit data pattern probably not helpful in this context
2022-09-29 7:02 AM
Yes, should work with HW, will need some clever initialization
/*
https://www.sciosense.com/wp-content/uploads/documents/SC-000897-DS-7-ENS210-Datasheet.pdf
*/
// 7654 3211
// Polynomial 0b 1000 1001 ~ x^7+x^3+x^0
// 0x 8 9
#define CRC7WIDTH 7 // 7 bits CRC has polynomial of 7th order (has 8 terms)
#define CRC7POLY 0x89 // The 8 coefficients of the polynomial
#define CRC7IVEC 0x7F // Initial vector has all 7 bits high
#define CRC7MASK ((1UL<<CRC7WIDTH)-1)
// Payload data
#define DATA7WIDTH 17
#define DATA7MASK ((1UL<<DATA7WIDTH)-1) // 0b 1 1111 1111 1111 1111
#define DATA7MSB (1UL<<(DATA7WIDTH-1)) // 0b 1 0000 0000 0000 0000
// Compute the CRC-7 of ‘val’ (should only have 17 bits)
uint32_t crc7(uint32_t val)
{
// Setup polynomial
uint32_t pol = CRC7POLY;
// Loop variable (indicates which bit to test, start with highest)
uint32_t bit = DATA7MSB;
// Align polynomial with data
pol = pol << (DATA7WIDTH-CRC7WIDTH-1);
// Make room for CRC value
val = val << CRC7WIDTH;
bit = bit << CRC7WIDTH;
pol = pol << CRC7WIDTH;
// Insert initial vector
val |= CRC7IVEC;
// Apply division until all bits done
while(bit & (DATA7MASK << CRC7WIDTH))
{
if (bit & val) val ^= pol;
bit >>= 1;
pol >>= 1;
}
return(val);
}Simplified
uint32_t crc7_test(uint32_t data) // ENS210 - sourcer32@gmail.com
{
int i;
uint32_t crc = ((data & 0x1FFFF) << 7) + 0x7F; // awkward initialization
for(i=0; i<17; i++)
{
if (crc & 0x800000) // 24-bit aligned
crc = (crc << 1) ^ (0x89 << 17); // align polynomial 24-7
else
crc <<= 1;
}
crc = (crc >> 17) & 0x7F; // shouldn't need masking
return(crc);
}
2022-09-29 8:15 AM
Mechanics for 32-bit implementation, ingesting 17-bit as singular word
uint32_t crc7_test32(uint32_t data) // ENS210 - EMU32HW - sourcer32@gmail.com
{
int i = 32;// width of crc
uint32_t init = 0x00000000; // yes, zero
uint32_t poly = (0x89 << (32 - 7)); // left align 32-bit
uint32_t crc;
data = (data & 0x1FFFF); // mask data word, or only 17-bits, right aligned
crc = data ^ init; // apply
while(i--)
{
if (crc & 0x80000000) // high order 32-bit
crc = (crc << 1) ^ poly;
else
crc <<= 1; // left shifting
}
crc = ((crc >> (32 - 7)) ^ 0x7F); // align, masked by left constraints, invert
return(crc);
} // sourcer32@gmail.comCould probably make the 7-bit HW work too, Initialize at ZERO, and INVERT output
2022-09-29 4:02 PM
Quick Parallel Version 7-bit CRC of 17-bit word
//******************************************************************************
uint32_t crc7_quick(uint32_t data) // CRC-7 ENS210 - sourcer32@gmail.com
{
static const uint32_t crctbl5[] = { // Polynomial 0x89 x^7+x^3+x^0
0x00000000,0x12000000,0x24000000,0x36000000,0x48000000,0x5A000000,// 0x00
0x6C000000,0x7E000000,0x90000000,0x82000000,0xB4000000,0xA6000000,// 0x05
0xD8000000,0xCA000000,0xFC000000,0xEE000000,0x32000000,0x20000000,// 0x0B
0x16000000,0x04000000,0x7A000000,0x68000000,0x5E000000,0x4C000000,// 0x11
0xA2000000,0xB0000000,0x86000000,0x94000000,0xEA000000,0xF8000000,// 0x17
0xCE000000,0xDC000000 };
uint32_t crc = data << (32 - 17); // left aligned
// 17 vis 3 rounds of 5 (15), 1 round of 2
crc = (crc << 5) ^ crctbl5[crc >> (32 - 5)];
crc = (crc << 5) ^ crctbl5[crc >> (32 - 5)];
crc = (crc << 5) ^ crctbl5[crc >> (32 - 5)];
crc = (crc << 2) ^ crctbl5[crc >> (32 - 2)];
return(~crc >> (32 - 7)); // inverted, left aligned, 7-bit
} // sourcer32@gmail.com
//******************************************************************************