STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Firmware MPU configuration and SBSFU FPU exceptions

It seems to be a recurring challenge in the community posts of getting firmware MPU configuration to work with SBSFU. We also had the problem of application firmware hanging when running it with SBSFU. A solution of clearing floating point unit flags...

sute by Associate III
  • 3269 Views
  • 5 replies
  • 0 kudos

How to exit safe mode for STM32H735.

How to exit safe mode when the security position of the chip is 1 and the protection area of the flash of the new chip is from 0x080000000 to 0x082020000, but the content in the flash is erased,Thank you.

wux by Associate
  • 1825 Views
  • 2 replies
  • 2 kudos

How to validate an image with security features enabled?

Hi all,In our project we have enabled the ENABLE_IMAGE_STATE_HANDLING flag and download an image via YMODEM transfer to our NUCLEO-L476RG. However, when we try to validate the image by calling SE_APP_ValidateFw(), our STM reboots and does a rollback....

ac_gd by Associate II
  • 13222 Views
  • 14 replies
  • 0 kudos

Resolved! File not correctly received - SBSFU

I am trying to follow the getting started guide (UM2262) for the SBSFU using our own hardware.  I have got as far getting to the main "secure boot and secure firmware update" screen in Tera Term, however when trying to send the .sfb file, I get the f...

Issue with SBSFU integration with custom user application

 Hi,I am trying to integrate custom user application with SBSFU bootloader for p-nucleo-WB55 and I was wondering in case anyone saw the following issue.When I try to use the Secure Engine functions for validation in my user application, the program g...

kaur by Associate III
  • 6673 Views
  • 11 replies
  • 0 kudos

Unable to set STM32U5 RDP password via USB interface

Hi,The STM32U5 has a password feature to restrict RDP regression from level 1 to level 0. However it seems that STM32CubeProgrammer CLI is unable to activate this via the USB interface of the built-in bootloader. If I do it via STLink then it works f...

AHugh.2 by Associate III
  • 2153 Views
  • 2 replies
  • 0 kudos

STM32U585 - Secure boot loader

Hello Everyone,We are currently working with STM32U585 microcontroller for one of our IoT project.In this project we are planning to implement secure boot.In this regard we want some clarification on the below points,1.  After doing secure firmware i...

Surya S by Associate II
  • 2269 Views
  • 2 replies
  • 3 kudos