User Activity

Good afternoon,we are facing issue with AES GCM Tag generated with STM32U585.In particular we compare the results generated by the microcontroller with the ones generated by an application developed with C#.This is the code running on the microcontro...
Good morning,we have a problem with ELF file loading. We are using an STM32U575 MCU on a Nucleo board.In particular:the location 0x0802A61B in the ELF file is set at 0x00 (we see it by open the ELF file with Cube Programmer).1) If we load the ELF fil...
Good morning to all,we are struggling with watchpoint feature. We have set up the watchpoint as showed in the picturebut the watchpoint never get triggered.We are using NUCLEOU575 board and we are debugging through the on board USB connector.We have ...
Hi all,we have successully used an external SPI memory to store images.We have defined an external Flash section in our linker file ExtFlashSection :{*(ExtFlashSection ExtFlashSection.*)*(.gnu.linkonce.r.*). = ALIGN(0x4);} >SPI_FLASH and then extract...
Hi all,we have developed an external loader to write a SPI flash. Start address is 0x9000000The loader was written following the ST procedure and disabling all interrupts.All works good but for file of dimension greater than 500k the download fail.Fo...