STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PCROP code calls to HAL functions

Hi, I have a firmware I wan't to give already flashed protected by PCROP to a customer. Insidie my firmware I use some standart library functions line strlen(), vsprintf and some HAL functions to manage peripherals.What is the best way to call these ...

mromani by Associate
  • 1030 Views
  • 1 replies
  • 0 kudos

STM32 X-CUBE-Cryptolib - IV length and padding

Hi everyone,I am trying to use the X-Cube-Cryptolib library to decrypt an array encrypted by an external application.The original data has been encrypted with the AES-GCM 128 using a key of 16 bytes and an IV of 1 byte.Now, I am getting an error wher...

AGhez by Associate III
  • 945 Views
  • 1 replies
  • 0 kudos

internal flash access using levelx

Hi, We are using STM32u585 device on our board, we want to use a part of internal flash memory for permanent data storage.  Please clarify the following. 1)is it possible to use internal flash access using LevleX (non RTOS)?2)is there any reference a...

Questions regarding the RAM self-test in X-CUBE-STL

When using the RAM self-test feature in X-CUBE-STL, I enabled the RAM backup buffer in the application by not defining STL_DISABLE_RAM_BCKUP_BUF. I also allocated a section in the scatter file:; 128KB DTCM RW_STL_TM_RAM 0x20000000 0x20 { ; Place STL...

Ryan_Lee by Associate
  • 1542 Views
  • 2 replies
  • 1 kudos

Resolved! STM32 cryptographic firmware library for STM32C071

Moved from MPUs forum: STM32C0 is an MCU - not an MPU. Hi, I am not sure if STM32 cryptographic firmware library can run on STM32C071 because this microcontroller does not have embedded Crypto (Hardware) ?   Thanks   Gregory Saint-Jean

GSain.1 by Associate II
  • 2029 Views
  • 4 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.