User Activity

Hi,STM32U585 + eMMC , by SDMMC2 busI want to configure the eMMC into sleep mode by HAL_MMC_SleepDevice API,but It does not workIt alway return 0 when I get the card state by HAL_MMC_GetCardState after run the API HAL_MMC_SleepDevice.Thanks!   
board: stm32U585 + stsafe-a110 before the stm32u585 enter the low power mode ,I want to set stsafe-a110 enter the low power consumpion mode. I can't find the methods to enter Hibernate      
Hi I have the project with the chip STSAFE_A110I don't need to development the application I just need to confirm the hardware is ok, for example, obtained the sn of the chip is successfully or other wayI don't want to add the stsw-safea1-mw to my pr...
board:MB1549-U575ZIQ-C03  (mcu stm32U575) I debug the FDCNA function with a CANalyst tool  1. Work at FDCAN_MODE_BUS_MONITORING mode, It can receive data from the CANalyst tool  2. Work at FDCAN_MODE_EXTERNAL_LOOPBACK,It can receive data itself and t...
Kudos given to