STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flashing an encrypted Firmware

Greetings, I am using a STM32U585 MCU and I made a custom made code that implements the DFU protocol. I could successfully flash a firmare through .bin file and set the Option Bytes, set RDP level 1 and go back to RDP level 0. What I want to do is to...

Resolved! TFM app

Hello,I would like to use the TFM application on STM32CubeIDE for the B-U585I-IOT02A board but I can't find the application anywhere. Any help?

SBSFU STM32U585 series with CMake toolchain

Hi everyone, I'm working on integrating the SBSFU (Secure Boot and Secure Firmware Update) into an existing project for a custom board using an STM32U585 microcontroller.At this stage of the project, I am trying to include the SBSFU_Boot (https://git...

Resolved! Can't access secure DCMIPP peripheral registers

Hello,I have a DCMIPP example application in FSBL that runs fine on an STM32N6570 Disco when loading it with the Disco board's built-in ST-Link. It has a DCMIPP_HandleType Def structure with hdcmipp.Instance that needs to access secure peripheral mem...

DBonh.1 by Associate III
  • 560 Views
  • 3 replies
  • 0 kudos

Resolved! Using RSSLib->DataProvisioning() interface without TZ

I'm trying to get the Debug Authentication provisioning to work. I managed to write it from within the application, but then I found the errata sheet(es0565-stm32h562xx563xx573xx-device-errata-stmicroelectronics.pdf) which states otherwise:"Chapter 2...

peter7 by Associate II
  • 1361 Views
  • 3 replies
  • 0 kudos

Resolved! Example code for SFIx variant of external loader

The following repository contains examples for creating 'normal' type of external loaders, i.e., to be used with the "-el" argument of the STM32CubeProgrammer (e.g., with output "STM32CubeProgrammer/bin/ExternalLoader/MX66UW1G45G_STM32H7S78-DK.stldr"...

Eliasvan by Associate III
  • 1107 Views
  • 1 replies
  • 2 kudos