STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32h533 production state closed firmware not running

Hello Support Team,for testing purposes i am using the H533NucleoBoard. I can load my firmware into the MCU and the firmware is running as expected. I want use the final product in ProductionState: closed.The problem is, the firmware isn't running an...

jhoerd by Associate II
  • 1629 Views
  • 2 replies
  • 1 kudos

Resolved! SFI Option Bytes for STM32H753ZI (Nucleo-H753ZI)

Hi everyone,I have a question regarding SFI Option Bytes for the STM32H753ZI (Nucleo-H753ZI).Question:Which option bytes should I pick, since there are a lot of different combinations available: 1. Generated by TrustedPackageCreator: FLASH_OPTSR_PRG,...

jho by Associate II
  • 1166 Views
  • 3 replies
  • 1 kudos

Secure Boot Implementation

HiI am trying to perform a secure boot implementation in STM32F439ZIT6. The datasheet shows that, there is Hash, RNG, AECS and TDES. Can I perform secure boot functionality using only STM32F439ZIT6 without using any external chip and if so, are there...

avbST by Associate II
  • 776 Views
  • 1 replies
  • 0 kudos

Resolved! Does STM32H743VIT6 has HASH peripheral?

 1.Does the STM32H743VIT6 microcontroller include a HASH peripheral that supports SHA-256 operations?I am planning to implement HMAC-SHA256 verification for my application, but I have not found clear documentation confirming the presence of a compati...

Anbu by Associate
  • 850 Views
  • 1 replies
  • 0 kudos

STM32H5 - X-CUBE-SEC-M-H5_V2.0.0 - CubeMX

Hi Everybody,I posted a comment here https://community.st.com/t5/stm32-online-courses/stm32h5-secure-manager-course/bc-p/824487/highlight/true#M27 yesterday because I am trying following the online course and what is written in the wiki to start deve...

andyi by Associate III
  • 1401 Views
  • 5 replies
  • 0 kudos

Resolved! STM32WBA63CUI7 OEM ROT Porting Help

 I'm porting OEM ROT examples from STM32WBA65I-DK1 to STM32WBA63CUI7 and need guidance.Devices:- Target: STM32WBA63CUI7 (2MB flash, CSP17)- Source: STM32WBA65I-DK1 (2MB flash, UFBGA169)Questions:1. Device Support: Any known STM32WBA63xx definition ga...

nomancy by Associate
  • 631 Views
  • 1 replies
  • 0 kudos

Resolved! OTA Secure Update using ESP32

Hello everyone,I would like to update the STM32 remotely using ESP32. So the Idea is to transfer the signed image via Bluetooth and to store it firstly on the esp32, which will transfer it in the end via UART to the STM32.After that the secure boot o...