STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F207 RNG

Hello,I'm having trouble using the RNG peripheral on the STM32F207.I'm using the HAL functions to set things up and I keep getting back the same number. I've made sure to enable the RNG Clock. See the steps below:Enabled RNG CLK: __RNG_CLK_ENABLE()En...

Anvi by Associate III
  • 6766 Views
  • 11 replies
  • 0 kudos

Button input value always keeps floating

Hi all, I am using button input from separate input (Separate PCB). After I disconnect that PCB, SBSFU automatically goes into the Updating mode. Even I tried to do an internal pull-up but it also doesn't work. I tried two methods of internal pull-up...

Roshan by Associate III
  • 2521 Views
  • 5 replies
  • 0 kudos

How to disable stm32g491 dual-bank mode

We were running tests originally with the g474re eval board to test/integrate SBSFU functionality. We needed to disable dual-bank mode with the STM32CubeProgrammer before being able to transfer via Ymodem. We are now trying on the g491 and are failin...

TDock.1 by Associate
  • 1203 Views
  • 1 replies
  • 0 kudos

Resolved! Memory limitations using SBSFU

Hello,I am developing a SBSFU for a custom application on a NUCLEO-H753ZI board. The application works well on its own. However, when I switch its linker script for the one of the example UserApp delivered with the SBSFU archive, I encounter some une...

EBonv by Associate III
  • 4369 Views
  • 8 replies
  • 0 kudos

Resolved! PCROP deactivation in STM32H7

I am working with STM32H750VBT6 rev. V. I divided the internal flash into protected and unprotected areas. I set option bytes for the protected area. It worked fine. After that I needed to deactivate PCROP protection. I could not do it. I use STM32Cu...

BEvge.1 by Associate II
  • 1689 Views
  • 1 replies
  • 0 kudos

I am learning about X-CUBE-AWS examples, when update from OTA, I get a SIGNATURE CHECK FAILED exception, somebody can help me to resolve this problem?

I download X-CUBE-AWS 1.4.0 to compile and install on my STM32F769IDISCOVERY board, everything running ok, but when I configure it to update new app version from OTA, after reboot is shows:= [SBOOT] SECURE ENGINE INITIALIZATION SUCCESSFUL= [SBOOT] ST...

saico by Associate II
  • 1641 Views
  • 2 replies
  • 1 kudos

Resolved! Cryptographic Acceleration STM32F207

Hello,The reference manual for the STM32F207 states that the F20x and F21x family has a cryptographic processor: Ref Manual - Page 508. The datasheet for the F207 doesn't state any support for that though. Is this a mistake in the reference manual?Th...

Anvi by Associate III
  • 1573 Views
  • 1 replies
  • 0 kudos

I am very very new in MPUs / MCUs and IOT. What product should I try for cryptographic operations like AES or Diffi Hellman and also for storing keys securely in device.

Hi, actually I 'm planning to write some C code for cryptographic functions for e-signature, encrypt data or decrypt data in IOT devices.There are lots of products here. So I don't know which one is efficient for encrypt or decrypt operations or sign...

OISLE by Associate
  • 1497 Views
  • 2 replies
  • 1 kudos

How to Program stm32f103rc using j-Link when RDP enabled?

Hello.I'm trying to program the main flash memory of STM32F103RCT6 using J-Link while RDP is enabled.I followed main flash memory programming procedure in PM0075 manual.the procedure is in below picture.When only RDP is enabled, I unlocked Flash_CR_L...

0693W00000Bd7ZLQAZ.png
HJung.2 by Associate II
  • 3379 Views
  • 3 replies
  • 0 kudos