STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Cannot Set DMA to Secure (CCRx SECM)

I'm attempting to configure peripherals in STM32CubeMX, but I'm getting error_handler calls from my DMA configuration for ADC1.All the necessary peripherals (DMA1 channel1, ADC1) are configured as secure in CubeMX, but when HAL_ADC_MspInit attempts t...

MBand.3 by Associate III
  • 1559 Views
  • 1 replies
  • 0 kudos

Resolved! In STM32L552 Nucleo-144, unable to load non secure code when call happened from secure to non secure.

I am working on STM32L552 Nucle0-144 board with Trustzone enabled. Secure code starts from 0x0C000000 and non secure code vector table located at 0x08040000. After completing the initializations in secure code I am calling non secure reset handler by...

MSatish by Associate II
  • 1446 Views
  • 2 replies
  • 0 kudos

from AWS IoT expansion package, ST use secure element STSAFE-A110. ST also provides middleware and SBSFU etc to support secure boot and AWS secure communication. My question is how difficult of using other secure element ATECC608A?

I think using other secure element should feasible, but not sure how difficult it is.As ST provides a set of tools like SBSFU etc middleware, may I know is that easy to change to support other secure element other than STFAFE-A110?

jiangpen by Associate II
  • 1043 Views
  • 1 replies
  • 0 kudos

Resolved! How to see the return value of the CRC_CalcCRC();

hi here I am configure the CRC register of STM32f469IITx I am using the function CRC_CalcCRC(); to generate the crc for 32-bit data.i am not getting the crc please any one help me.uint32_t data=0xAAAAAAAA;uint32_t crcvalue=0x00000000;how i am using ...

Trinu by Associate III
  • 1293 Views
  • 2 replies
  • 0 kudos

Resolved! SBSFU integration with stm32f407g-disc1 (stm32f407vgt6u)

Hello,The mentioned board utilizes usb otg communication through the USB connector. DM and DP pins are PA11 and PA12 which are directly connected from the mcu to the USB connector (no available GPIO pins). There is no usart or uart connected to the D...

AArzo.1 by Associate
  • 1706 Views
  • 2 replies
  • 0 kudos

how to unlock stm32f103c8 write protection

I have set readout protection,the f103c8 chip have automatically set the first four page write protect,now I wanna erase the first four page,how can I unlock write protection first,thank you

kluna.1 by Associate
  • 1146 Views
  • 0 replies
  • 0 kudos

Resolved! X-CUBE-SMBUS Middleware not supported for STM32F407

Is there any way to use the X-CUBE-SMBUS middleware from ST with STM32F407?The controller does support it but ST's middleware does not.Does anyone know why it would not be supported?The reason I say its not is because the HAL for it is not in the #if...

Nandan V by Associate II
  • 1830 Views
  • 2 replies
  • 0 kudos