STM32 MCUs Other solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Host Audio Class- how to handle

Hello,Is there any working example of USB Host Audio Class? I am trying to run it using the API but I am having some hard time. In repository there is no example (in any repository) and there are no user manuals.I am able to connect to the USB Audio ...

maciek by Associate II
  • 297 Views
  • 1 replies
  • 0 kudos

How to set required voltage on STUSB4500 IC

Hello     Requirement is:we are using 3 cell(3.7*3 = 11.1V) battery in our design.so we are using charging IC for that.charging IC need 15v(max 2A) to charge LIPO battery.so we are going to use universal type c charger that Supports 5V,9V,12V, 15V an...

Apate.61 by Associate
  • 278 Views
  • 1 replies
  • 0 kudos

Resolved! Code Isolation for Functional Safety

HI,  I am considering the use of STM32F0 device for my project. How do I isolate the safety related code(for functional safety)  from the general code, so that a f/w update on the general code doesn't affect the safety related code? Are there any har...

arthiJan by Associate II
  • 1451 Views
  • 18 replies
  • 1 kudos

Using PDM to PCM conversion library

I am using a STM32L1 MCU and I want to use the PDM to PCM conversion library, so I downloaded X-CUBE-MEMSMIC1, in the audio PDM lib folder I found libPDMFilter_CM3_Keil.lib. In the release note I read this lib is for 16KHz PCM data sampling rate, So ...

J Lee by Associate III
  • 975 Views
  • 4 replies
  • 0 kudos