STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1745 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4896 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9603 Views
  • 5 replies
  • 3 kudos

How to use BEMF Example source

I am developing something using STEVAL-SPIN3202 Development KitIt support BEMF however, 0x35{Observer BEMF alpha (PLL)} value has not been changed at ST Motor Control workbench. How can i use it?In addition, I only found Potentiometer and Uart in exa...

SKwon.2 by Associate
  • 1489 Views
  • 2 replies
  • 0 kudos

Isn't this a bug in X-CUBE-SPN8 ?

I've been working on BLDC motor control using STM32F302R8 with X-CUBE-SPN8. I've found there occurs wrong ADC conversion frequently. Thinking this comes from that the LFtimer period which is related to step changes and varies with motor speed, is not...

TChun.11 by Associate
  • 869 Views
  • 1 replies
  • 0 kudos

overspeed problem

Overspeed problemI purchased evspin32f0601s3 board. Running the motor seems to be more responsive than evspin32f0601s1. But there is the same problem at start. It is that it takes overspeed. In my opinion, there seems to be a problem with the feedbac...

0693W000007BitFQAS.jpg
DLee.10 by Associate
  • 1156 Views
  • 1 replies
  • 0 kudos

trying to compile the en.STSW-SPIN32F060x.zip project.

I am trying to compile the en.STSW-SPIN32F060x.zip project.However, even if I generate the code with MDK-ARM 5, cubeIDE, etc. in CubeMx and compile it with the corresponding compiler, it is difficult to generate the hexa file due to various errors......

DLee.10 by Associate
  • 960 Views
  • 1 replies
  • 0 kudos

"Rebond" problem at 0 Speed

I have a bounce problem close to 0 speed,I modified the software filter of the halls sensors in MC without results, obviouly i have ajust motor settings, voltage, current, and main settingsdo you know where this problem may come from ?I'm working on ...

RFouj.1 by Associate
  • 1118 Views
  • 1 replies
  • 0 kudos

How to connect STEVAL-PTOOL2V1

Hello,My STEVAL-PTOOL2V1 has OUTU OUTV OUTW but my BLDC has MA MB MC. How do I connect.My STEVAL-PTOOL2V1 has A+/H1 B+/H2 Z+/H3 by my BLDC has HA HB HC. How do I connect.

ADani.2 by Associate III
  • 1038 Views
  • 1 replies
  • 0 kudos