STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G0: cannot activate GPIOB AND GPIOD

I have an other issue at the moment. I cant use the GPIOD, VSSI02 is on 3.3V. Im using stm32g0b1kb. It wont toggle it wont read, it does nothing. I have created a small application far away from my main app just to test the GPIO functions.Hi, I a alr...

kuda1311 by Associate II
  • 1221 Views
  • 11 replies
  • 5 kudos

Dual bank booting problem

Hello!I try to use dual bank option on the stm32l476 (256kB) for implementing a custom bootloader. I want just read new program (bin) by custom protocol and write it to another bank. After that I want to switch the banks, reset mcu and start the new ...

KKlyn.1 by Associate II
  • 3902 Views
  • 5 replies
  • 1 kudos

Unable to get the IP using DHCP

Hello everyone,   I am trying to get an IP for my controller using the DHCP i can able to detect the Link up and link down but i can't able to get the IP. I had refered the example code for the ethernet(lwip https server netconn rtos) But i can't abl...

HELP with Burst Mode HRTIM

  Hi everyone, I am working on an STM32G4 project using the HRTIM1 peripheral. My goal is to generate a burst of exactly 3 PWM pulses on Timer A and Timer B simultaneously, triggered by an External Event (Sync Input / EEV). The Goal: System waits fo...