STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L151ZD Bootloader Options

Posted on June 26, 2012 at 16:48I'm having difficulty finding a definite answer to my question in the forums or the application notes.We were hoping to use the USB to allow us to download our target firmware to our product, thus not requiring our us...

DFUSe Crashing when modifying option bytes

Posted on May 23, 2012 at 17:58Hi, I am trying to modify the option bytes of my ST so I can disable and enable write protection;however, when I am using DfuSe demo it crashes, I am wondering if anybody else has encountered the same issue, or have a ...

Data dropout in VCP USB application

Posted on June 27, 2012 at 05:20Hi,I am working on a vibration sensor project where I need to send data from an accelerometer over USB to a computer application with a data loading of about 24 bytes per millisecond. I am using using a custom-built S...

Pygmt OS is recruiting open source contributors

Posted on June 26, 2012 at 08:07Hi, my name is Warren Greenway, founder of Pygmy OS and the Pygmy Project. We are currently looking for a few good developers to join the core team in preparation for our first stable public release. Pygmy OS is an RT...

warrend by Associate
  • 983 Views
  • 2 replies
  • 0 kudos

USB Mass Storage Demo Problems

Posted on September 20, 2011 at 21:51Hi,I am working with the STM3210C-EVAL Board and the demos provided with the STM32F105/7 and STM32F2xx USB on-the-go Host and device library.The libraries provided for initializing the USB on the device take a st...

USB input pins

Posted on June 15, 2012 at 12:32Where is the USBDM and USBDP (pins name for USB) defined under standard library files from stm. I have a microcontroller with USBDM and USBDP as PA11 and PA12. I would like to know in which header file the corresondin...