STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeF0 Bug Report - __HAL_REMAP_PIN_ENABLE

Posted on March 04, 2015 at 23:46I tried to configure the CAN controller in the STM32F042F6P6 using STM32CubeMX. The function was not correct because it was not properly remapping pins PA11, PA12. Macro __HAL_REMAP_PIN_ENABLE does not activate SYSC...

f_open error 11 (can't find FR_INVALID_DRIVE)

Posted on March 02, 2015 at 01:47My issue is with fatfs in the following code:retSD = FATFS_LinkDriver(&SD_Driver, SD_Path);if(retSD == 0) { if(f_mount(&sdcard,(TCHAR const*)SD_Path,1) != FR_OK) //works great { Error_Handler(); } else { //HAL_SD_Wid...

STM32F107 ethernet demo rebuild problem

Posted on February 27, 2015 at 16:31Has any body rebuilt the STM32F107 LwIP TCP/IP demo (STSW-STM32026)   in latest IAR EWARM toolchain ? The demo provided by ST still uses IAR 5.42 ( old one). This creates errors when I try to rebuild with IAR 6.30...

jay by Associate
  • 2021 Views
  • 4 replies
  • 0 kudos

Triple mode ADC with new HAL

Posted on December 01, 2014 at 22:52 Hello, I'm trying to set the ADC(s) of the stm32f407 in triple mode, using DMA for data transfers. Based on the the only available example in the cube package and some old code, written using the stdpheri...

b2527456 by Associate II
  • 2955 Views
  • 5 replies
  • 0 kudos

STM32F207 USB device with no VBUS monitoring

Posted on June 10, 2014 at 09:05Hi all,I'm modifying the VCP demo for STM32F207 to work without VBUS sensing, just using D+/D- for USB communications. As stated in RM0033 (page 935/1334 Doc ID 15403 Rev 5, chapter 29.5 USB peripheral): �The VBUS pin...