STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7 Ethernet operation TE vs. ETH_TX_EN

Posted on December 08, 2016 at 22:38Hi all, I'm working with Ethernet on an STM32F745IETx and with a project configured using STM32CubeMX. We're using an RMII interface to a chip that supports three Ethernet ports. I've tested pass through between t...

hbarta2 by Associate III
  • 1274 Views
  • 2 replies
  • 0 kudos

examples in Cube

Posted on November 27, 2016 at 03:51 Anyone figure out how to run the examples downloaded with Cube ? I am using the f0, r8 chip with the nucleo board. I have been programming using bare metal (registers) and some spl to learn about the chip. No pr...

STM32 HAL UART transmission

Posted on December 08, 2016 at 09:38 I'm trying to send data by STM32f103 to an Arduino board using UART. Data isn't received properly. The code is generated using STM32CUBEMX and here is the part I added: uint8_t Test[] = '1 2 3 4 5 6 7 8 9 1...

kmehranh by Associate II
  • 1761 Views
  • 2 replies
  • 0 kudos

Purpose of dedicated DMA for USB and how does it work

Posted on December 06, 2016 at 20:42Hi.I started to work with STM32F7 series and USB HS (CDC class). I am able to send data to PC using CDC_Transmit_HS(uint8_t* Buf, uint16_t Len) function, but I am not aware what is going on behind it. If let say, ...

matic by Associate III
  • 6538 Views
  • 5 replies
  • 0 kudos

Custom bootloader STM32F405VG

Posted on November 26, 2016 at 00:33Hello,I'm working in a custom bootloader. I have follow many discussions here and then i end up with this code.commenting the function PerformFirmwareUpdate() the code works ok!   pFunction appEntry; uint32_t appS...

abarrotes by Associate II
  • 5570 Views
  • 14 replies
  • 0 kudos