STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F334 SPI

Posted on August 29, 2016 at 14:02Hi! I am new to STM32 microcontrollers and SPI. I'm currently working on STM32F334R8T6 (Nucleo board 64-pin package) and need to configure it as spi full duplex master without crc for operating MAX31865 temperature ...

vishi100 by Associate II
  • 3206 Views
  • 6 replies
  • 0 kudos

Smoke Alarm Tone Detection Using STM32F407

Posted on July 13, 2017 at 12:35Hello All,Application Requirement:   Alarm detection using STM32F407 discovery Board and if alarm tone detect generate alarm signaland system become off.Issue :1> While Mic Place on the Loudspeaker alarm tone detect a...

chintan by Associate
  • 1163 Views
  • 0 replies
  • 0 kudos

STM32F4 Cycles Fluctuation With Network

Posted on July 13, 2017 at 12:15https://stackoverflow.com/questions/44964999/stm32f4-cycle-fluctuations?noredirect=1 Hi,I have STM32F4 running with FreeRTOS and LwIP for networking library. I want to know how much cycle that STM32F4 needs when it re...

rama by Associate
  • 1043 Views
  • 0 replies
  • 0 kudos

Resolved! VCP device doesn't receive from C# app

Posted on June 29, 2017 at 17:49Hello the STM Community,To quickly introduce my setup, I work on a custom board with a STM32f407 but I have the same issue with the STM32f4-discovery. I generate a simple project for this card, only to try the USB-OTG...

Resolved! LwIP DHCP no ip request

Posted on July 11, 2017 at 18:17Hello fellow STM32 explorersI am currently working on a STM32F4 TCP/IP project.I'm using LwIP's RAW api.I got a echo UDP program working but with a static IP now I'm trying to get an ip adress automatically using a DH...

andy b by Senior
  • 2248 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L471 DFU

Posted on July 12, 2017 at 07:55I'm confused about wether STM32L471RG has a USB bootloader or not. AN2606 describes an STM32L47xxx DFU bootloader and that USB DM and USB DP lines should be connected to PA11 and PA12 respectively.But what confuses me...

0690X00000607H5QAI.png 0690X00000607YsQAI.png

playback wave file with DMA on STM32F745VGT6

Posted on July 11, 2017 at 17:23Hi Communities,I am using STM32F745VGTX Chip for my audio playing wave file application. My problem is that playing wave file takes too much processor power, therefore I want to use DMA instead. Is there any DMA mode,...

PC Connection detect using FTDI chip

Posted on July 06, 2017 at 15:40Hello,I am working on Stm32l073 series controller. I have small question regarding the deep sleep and exit from deepsleep modes when device is not plugged to PC i must make the device go to sleep. As the Block Diagram...

0690X00000607SkQAI.png
srm by Associate II
  • 2565 Views
  • 4 replies
  • 0 kudos