Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Posted on July 29, 2014 at 01:49Hi i'm new using ARM architecture i bought the STM32F4 Discovery Evaluation Card, it stop working after trying to load my first program, the demostration code no longer runs, the only thing is doing when i plug the US...
Posted on July 24, 2014 at 12:08 Hi, I'm trying to program http://andybrown.me.uk/wk/wp-content/images//awreflow/schematic.pdf with a stm32f0308-disco st-link but it only works if I power the board with the 3v from the disco board if I po...
Posted on June 24, 2014 at 08:36 I am downloading file to chip with stlink/V2, the command line tool works fine for me.However, if the chip is on protect statue, the command line tool failed with below log:>>> Erasing PROGRAM MEMORYThe device is pr...
Posted on June 12, 2014 at 06:50Hi,I am planning to use STM32 series microcontroller (http://www.st.com/web/catalog/mmc/FM141/SC1169/SS1031/LN1565/PF164476) in my project. Wondering if anyone has footprint library for LQFP48 package. I am designing ...
Posted on May 10, 2014 at 01:24I have no problem using Utility v3.1.0 and firmware V2.J17.S0 with a Discovery-F3. I'm having a problem with v3.3.0 (the latest) with firmware V2.J19.S0. Most everything works except that the MCU Core Panel dialog fail...
Posted on April 19, 2014 at 16:52Hi there, I've designed a board on stm32f407zgt6 earlier and succeeded to connect my board with st link. All SWD connections were directly taken out from controller with no external pull-ups or pull-downs. Now again ...
Posted on March 24, 2014 at 02:43Hi all, I am using the STM32's ITM to output log messages to my PC via SWO. However, I have run into issues with losing characters (as has been noted elsewhere; e.g., /5056d518). Apparently ST-LINK fw V2.J19.S0 imp...
Posted on June 18, 2012 at 20:59Hi to all STM guys here. Thank for all the great eval boards you do.We just had a sparks-generating discussion on a forum from where camse an idea that we miss an interaction with PC capability on the discovery boards...
Posted on April 19, 2013 at 18:11Hi, for an automatic test, i need to Halt and Run a STM32. It works without problems with the STM32 ST-LINK Utility, but not (program is still running) when I use the CLI (st-link_cli.exe) in this way:st-link_cli.e...
Posted on January 23, 2014 at 14:00Hi All, I've ported the VCP to F3DISCOVERY ([DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/STM32F3DISCOVERY%20USB%20CDC%20%28Virt...