Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STUSB4500L Schematics review + questions

Hello all,I am attaching the schematics for a PD sink system we have designed and built. Our aim is to get this sink system to accept both PD and non PD type C power supplies and transfer their power to the 'FRONT_PWR' path on our schematics.Of cours...

NDvas.3 by Associate III
  • 1976 Views
  • 2 replies
  • 1 kudos

Resolved! Where can I download the BlueNRG stack images?

I have been searching through the ST website to try to find the BlueNRG stack image v2.1c (the bluetooth 5.2 compliant version). If I search "stage image" under the "Tools and Software" section, I get results for other versions (such as STSW-BNRG-V63...

BPaik by Senior
  • 3451 Views
  • 6 replies
  • 2 kudos

Resolved! Need details for USB Interface IC DRP

Here I'm using a USB Interface IC DRP for OTG. when I look into the datasheet for interfacing, I find some details in the pinout contrary to the diagram for pin numbers 16 and 17. Please someone clarify in this  

AravindR_0-1691125297024.png AravindR_1-1691125349801.png
Aravind R by Associate II
  • 1840 Views
  • 2 replies
  • 1 kudos

Sending data using BLEUNRG-2

Hello,I program a BLE, I can send and receive data with the ST BLE Toolbox application.I want to use another application that is not programmed by the ST community to communicate with my server, I can receive data from this application but I cannot s...

AMACH.1 by Associate II
  • 722 Views
  • 0 replies
  • 0 kudos

Resolved! TESEO LIV3F IO Supply Voltage

Hello,I would like to connect a TESEO LIV3F to an STM32 MCU that is powered using a 2.4v supply.Im wondering if I can drive TESEO's Vcc_io with a 2.4v supply or if I should use a 3.3v according to the datasheet and put a level shifter between them bo...

ABouk.1 by Associate III
  • 5327 Views
  • 10 replies
  • 1 kudos

Resolved! S2LP sniff mode

Hi,I successfully configured the transceiver RX mode with RX always ON.Now I'm trying to use Sniff mode. Basically I copied the example from S2LP DK.   // Below the code relevant for sniff mode. Initial radio, packet and address // configu...

Evgeny M by Associate II
  • 1815 Views
  • 1 replies
  • 0 kudos