Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STUSB4500 2.7V Supply Specs

I am interested in using the built-in 2.7V LDO on the STUSB4500 to power other parts of my circuit. Do you have any information on how much current this pin can source? And is the LDO hooked up to whatever VUSB is set to? For example, if the circuit ...

L9637

Hi,I would like to know if L9637 transceiver can be used with LIN protocol.I would also like to know if this transceiver can be used in a system bus where there are many Electronic Control Units (ECUs) and their communication is through of K-line and...

Aarong by Associate
  • 779 Views
  • 0 replies
  • 0 kudos

TESEO: 3D-Fix, wrong position at low SNR

Dear all.I am working together with a company facing a problem with TESEO-GNSS-Receiver in Japan. In an automotive usecase, with low SNR, the receiver gives us a wrong position, we've seen it off by up to 200 Meters. This alone would not be too bad, ...

VD6283TX ALS not working properly

Hi ,I am working on STM32L0 series controller with VD6283TX ALS on I2C interface.Though code is available for the sensor, my requirement is to write own code that will control the sensor. Sometimes it reads the RAW data from sensor and sometimes it ...

BChav.1 by Associate III
  • 3194 Views
  • 3 replies
  • 0 kudos

eSim

Hi, I am looking for typical application in the datasheet (for example - ST4SI2M0020TPIFW) and and find nothing. Do you have some typical schema? What does the eSim connect to? What else is needed in the way to the processor? Thanks for examples

RomanD by Associate
  • 920 Views
  • 0 replies
  • 0 kudos